MCUXpresso SDK Documentation

MCUXpresso SDK Changelog#

Board Support Files#

board#

[25.06.00]#

  • Initial version

clock_config#

[25.06.00]#

  • Initial version

pin_mux#

[25.06.00]#

  • Initial version

AOI#

[2.0.0]#

  • Initial version.

CADC#

[2.2.0]#

  • New Features

  • Supported platforms which don’t have ANA4 expansion MUX.

[2.1.0]#

  • Improvements

  • Added some APIs to support some devices that equipped expansion mux.

[2.0.1]#

  • Bug Fixes

  • Fixed the bug that channel mode set to wrong value.

  • Fixed the bug that independent parallel mode set to wrong value.

  • Fixed violations of the MISRA C-2012 rules.

[2.0.0]#

  • Initial version.

CLOCK#

[2.1.0]#

  • Accumulated bug fix

  • MISRA warning fix

[2.0.0]#

  • Initial version.

CMP#

[2.0.1]#

  • Improvements

  • Supported MC56F82xxxx and MC56F84xxxx.

    • Bug Fixes

  • Fixed violations of the MISRA C-2012 rules.

[2.0.0]#

  • Initial version.

COMMON#

[2.6.7]#

  • Improvements

    • EnableIRQ/DisableIRQ: Use IRQSTEER_GetInstIdxByIRQ() to determine IRQSTEER instance index instead of simple division. Supports multiple IRQSTEER instances with different interrupt counts.

[2.6.6]#

  • Improvements

    • Support Cortex M55.

[2.6.5]#

  • Bug Fixes

    • Fixed the issue that the function SDK_DelayAtLeastUs may underflow and cause a long delay when the input parameter is small and the system clock is low.

[2.6.4]#

  • New Features

    • Add macros to tag deprecated features and experimental features.

[2.6.3]#

  • New Features

    • Added bit mask inversion macros to avoid type promotion.

    • Added register operation macros.

  • Improvements

    • Make function MSDK_EnableCpuCycleCounter compatible with CMSIS-5 and CMSIS-6.

  • Bug Fixes

    • Fixed build issue of CMSIS PACK BSP example caused by CMSIS 6.1 issue.

[2.6.2]#

  • Bug Fixes

    • Fixed violations of MISRA C-2012 rule for implicit conversions in boolean contexts

[2.6.1]#

  • Improvements

    • Support Cortex M23.

[2.6.0]#

  • Bug Fixes

    • Fix CERT-C violations.

[2.5.0]#

  • New Features

    • Added new APIs InitCriticalSectionMeasurementContext, DisableGlobalIRQEx and EnableGlobalIRQEx so that user can measure the execution time of the protected sections.

[2.4.3]#

  • Improvements

    • Enable irqs that mount under irqsteer interrupt extender.

[2.4.2]#

  • Improvements

    • Add the macros to convert peripheral address to secure address or non-secure address.

[2.4.1]#

  • Improvements

    • Improve for the macro redefinition error when integrated with zephyr.

[2.4.0]#

  • New Features

    • Added EnableIRQWithPriority, IRQ_SetPriority, and IRQ_ClearPendingIRQ for ARM.

    • Added MSDK_EnableCpuCycleCounter, MSDK_GetCpuCycleCount for ARM.

[2.3.3]#

  • New Features

    • Added NETC into status group.

[2.3.2]#

  • Improvements

    • Make driver aarch64 compatible

[2.3.1]#

  • Bug Fixes

    • Fixed MAKE_VERSION overflow on 16-bit platforms.

[2.3.0]#

  • Improvements

    • Split the driver to common part and CPU architecture related part.

[2.2.10]#

  • Bug Fixes

    • Fixed the ATOMIC macros build error in cpp files.

[2.2.9]#

  • Bug Fixes

    • Fixed MISRA C-2012 issue, 5.6, 5.8, 8.4, 8.5, 8.6, 10.1, 10.4, 17.7, 21.3.

    • Fixed SDK_Malloc issue that not allocate memory with required size.

[2.2.8]#

  • Improvements

    • Included stddef.h header file for MDK tool chain.

  • New Features:

    • Added atomic modification macros.

[2.2.7]#

  • Other Change

    • Added MECC status group definition.

[2.2.6]#

  • Other Change

    • Added more status group definition.

  • Bug Fixes

    • Undef __VECTOR_TABLE to avoid duplicate definition in cmsis_clang.h

[2.2.5]#

  • Bug Fixes

    • Fixed MISRA C-2012 rule-15.5.

[2.2.4]#

  • Bug Fixes

    • Fixed MISRA C-2012 rule-10.4.

[2.2.3]#

  • New Features

    • Provided better accuracy of SDK_DelayAtLeastUs with DWT, use macro SDK_DELAY_USE_DWT to enable this feature.

    • Modified the Cortex-M7 delay count divisor based on latest tests on RT series boards, this setting lets result be closer to actual delay time.

[2.2.2]#

  • New Features

    • Added include RTE_Components.h for CMSIS pack RTE.

[2.2.1]#

  • Bug Fixes

    • Fixed violation of MISRA C-2012 Rule 3.1, 10.1, 10.3, 10.4, 11.6, 11.9.

[2.2.0]#

  • New Features

    • Moved SDK_DelayAtLeastUs function from clock driver to common driver.

[2.1.4]#

  • New Features

    • Added OTFAD into status group.

[2.1.3]#

  • Bug Fixes

    • MISRA C-2012 issue fixed.

      • Fixed the rule: rule-10.3.

[2.1.2]#

  • Improvements

    • Add SUPPRESS_FALL_THROUGH_WARNING() macro for the usage of suppressing fallthrough warning.

[2.1.1]#

  • Bug Fixes

    • Deleted and optimized repeated macro.

[2.1.0]#

  • New Features

    • Added IRQ operation for XCC toolchain.

    • Added group IDs for newly supported drivers.

[2.0.2]#

  • Bug Fixes

    • MISRA C-2012 issue fixed.

      • Fixed the rule: rule-10.4.

[2.0.1]#

  • Improvements

    • Removed the implementation of LPC8XX Enable/DisableDeepSleepIRQ() function.

    • Added new feature macro switch “FSL_FEATURE_HAS_NO_NONCACHEABLE_SECTION” for specific SoCs which have no noncacheable sections, that helps avoid an unnecessary complex in link file and the startup file.

    • Updated the align(x) to attribute(aligned(x)) to support MDK v6 armclang compiler.

[2.0.0]#

  • Initial version.

COP#

[2.2.3]#

  • Bug Fixes

    • Fixed violations of MISRA C-2012 rule 10.3.

[2.2.2]#

  • Bug Fixes

  • Added configuration of CWP bits in COP_Init, fixed write protection bEnableWriteProtect cannot be configured as part of cop_config_t.

[2.2.1]#

  • Bug Fixes

  • Fixed violations of the MISRA C-2012 rules.

[2.2.0]#

  • Improvements

  • Updated cop_config_t member naming.

  • Deleted COP_Disable API, added COP_Enable to enable/disable COP.

[2.1.0]#

  • Improvements

  • API interface changes:

    • Renamed “COP_EnableInterrupts/COP_DisableInterrupts” to “COP_EnableInterrupt/COP_DisableInterrupt” and remove unnecessary parameter.

    • New Features

  • Added APIs to enable/disable the COP COP Loss of Reference counter.

[2.0.0]#

  • Initial version.

CRC#

[2.0.0]#

  • Initial version.

DAC#

[2.0.1]#

  • Improvements

  • Supported MC56F82xxx and MC56F84xxx.

    • Bug Fixes

  • Fixed violations of the MISRA C-2012 rules.

[2.0.0]#

  • Initial version.

DMA#

[2.0.1]#

  • New Features

    • Added common IRQ handler entry DMA_DriverIRQHandler.

[2.0.0]#

  • Initial version.

EWM#

[2.0.2]#

  • Bug Fixes

  • Fixed violations of MISRA C-2012 rule 10.3.

[2.0.1]#

  • Bug Fixes

  • Fixed violations of the MISRA C-2012 rules.

[2.0.0]#

  • Initial version.

FLASH#

[3.0.0]#

  • Initial version — Basic FTFx IP command support

GPIO#

[2.0.1]#

  • Bug Fixes

  • Fixed violations of the MISRA C-2012 rules.

[2.0.0]#

  • Initial version.

I2C#

[2.0.2]#

  • New Features

    • Added common IRQ handler entry I2C_DriverIRQHandler.

[2.0.1]#

  • Bug Fixes

  • Fixed violations of the MISRA C-2012 rules.

[2.0.0]#

  • Initial version.

INTC#

[2.0.2]#

  • Improvements

    • Support SOC with different vector base address (VBA) shift.

[2.0.1]#

  • Improvements

  • Added doxygen comments.

[2.0.0]#

  • Initial version.

MCM#

[2.1.0]#

  • Improvements

    • Supported MC56F85xxx.

[2.0.1]#

  • Improvements

  • Supported MC56F82xxx and MC56F84xxx.

[2.0.0]#

  • Initial version.

MSCAN#

[2.1.1]#

  • New Features

    • Added common IRQ handler entry MSCAN_DriverIRQHandler.

[2.1.0]#

  • Improvements

    • Added wrong data length code(DLC) detection, report kStatus_MSCAN_DataLengthError when DLC is wrong.

[2.0.1]#

  • Bug Fixes

    • Fixed violations of MISRA C-2012 rule 10.3.

[2.0.0]#

  • Initial version.

PIT#

[2.3.3]#

  • Bug Fixes

  • Fixed CERT INT31-C violations in the CTRL register accesses: complements of 16-bit register masks are now explicitly cast to uint16_t before the read-modify-write, and the bool bEnableNegativeEdge field is normalized to 1U/0U before the PIT_CTRL_PRESET_POLARITY() write.

[2.3.2]#

  • Improvements

  • Guarded slave mode support (pit_config_t.bEnableSlaveMode, PIT_EnableSlaveMode(), and the CTRL SLAVE bitfield write) behind FSL_FEATURE_PIT_CTRL_HAS_SLAVE so devices whose PIT CTRL has no SLAVE bit build correctly.

[2.3.1]#

  • Bug Fixes

  • Fixed violations of MISRA C-2012 rule 10.3.

[2.3.0]#

  • Improvements

  • Filtered Preset input to reset PIT counter.

  • Support SYNC_OUT output stretch and toggle mode.

  • Added PIT_SetPresetFiltConfig() to set FILT register configurations.

  • Added PIT_SetSyncOutConfig() to set SYNC register configurations.

[2.2.1]#

  • Bug Fixes

  • Fixed violations of the MISRA C-2012 rules.

[2.2.0]#

  • Improvements

  • Updated pit_config_t member naming.

  • Removed some APIs for prescaler and clock source selection.

[2.1.0]#

  • Improvements

  • Updated PIT clock source and PIT prescaler with more meaningful comments.

  • Updated PIT_SetTimerPeriod() and PIT_GetCurrentTimerCount() with 16-bit parameter.

  • Deleted mask parameter for PIT_ClearStatusFlags/PIT_EnableInterrupts/PIT_DisableInterrupts.

  • Added PIT_SetTimerClockSource() API to configure clock source.

  • Added PIT_EnableSlaveMode() API to configure slave mode.

[2.0.1]#

  • New Features

  • Added PIT_SetTimerPrescaler() API to configure clock prescaler value.

[2.0.0]#

  • Initial version.

PMC#

[2.1.0]#

  • Improvements

  • Added PMC_SetVrefTrim() and PMC_SetVcapTrim() APIs to support MC56F80xxx.

[2.0.0]#

  • Initial version.

eFlexPWM#

[2.2.1]#

  • Bug Fixes

    • Fixed PWM_SetupFaultProtectionConfig() using wrong macro PWM_FCTRL_FSAFE instead of PWM_FCTRL_FIE for the fault interrupt enable field.

    • Fixed PWM_SetupFaultProtectionConfig() using PWM_FFILT_GSTR for both FILT_CNT and FILT_PER fields instead of PWM_FFILT_FILT_CNT and PWM_FFILT_FILT_PER.

    • Fixed PWM_SetupOutputConfig() not programming TCTRL[OUT_TRIG_EN] bits from bVal0TriggerEnable ~ bVal5TriggerEnable; previous code overwrote TCTRL multiple times and lost the OUT_TRIG_EN value.

    • Fixed PWM_SetupOutputConfig() not updating MASK register on devices without MASK[UPDATE_MASK] bitfield.

    • Fixed PWM_SetupSMConfig() passing the address of eStrBusClock (&psConfig->eStrBusClock) instead of its value to PWM_MCTRL2_STRETCH_CNT_PRSC(), and using |= which preserved stale prescaler bits; corrected to RMW.

    • Fixed PWM_SetupDeadtimeConfig() leaving CTRL[SPLIT] set when switching away from kPWM_IndependentWithSplitDoubleSwitchPwm mode.

[2.2.0]#

  • New Features

  • Supported capture PWM input filter.

  • Supported different PWM deadtime count register width.

    • Bug Fixes

  • Fixed wrong pwm_sm_pwm_out_t enum order issue.

[2.1.1]#

  • Bug Fixes

  • Fixed build error when soc not support Capture A/B features.

[2.1.0]#

  • Improvements

  • Supported MC56F80xxx.

[2.0.2]#

  • Bug Fixes

  • Fixed clear status flags API doesn’t work issue.

[2.0.1]#

  • Improvements

  • Supported MC56F82xxx and MC56F84xxx .

    • Bug Fixes

  • Fixed violations of the MISRA C-2012 rules.

[2.0.0]#

  • Initial version.

QSCI#

[2.0.5]#

  • New Feature

    • Added common IRQ handler entry QSCI_DriverIRQHandler.

[2.0.4]#

  • Bug Fixes

  • Fixed DMA transfer blocking issue by enabling tx idle interrupt after DMA transmission finishes, and invoke completion callback after tx idle interrupt occurs.

[2.0.3]#

  • Bug Fixes

  • Fixed violations of the MISRA C-2012 rules.

[2.0.2]#

  • Improvements

  • Supported QSCI which has 13-bit integer and 3-bit fractional baud rate selection.

[2.0.1]#

  • Bug Fixes

  • Fixed bug that when starting the non-blocking receive, the rx idle interrupt is not enabled, and when receiving is done the rx idle interrupt is not disabled.

[2.0.0]#

  • Initial version.

QTMR#

[2.0.1]#

  • Improvements

  • Supported to get TMR capture register address.

    • Bug Fixes

  • Fixed violations of the MISRA C-2012 rules.

[2.0.0]#

  • Initial version.

Queued SPI#

[2.1.2]#

  • New Feature

    • Added common IRQ handler entry QSPI_DriverIRQHandler.

[2.1.1]#

  • Bug Fixes

  • Fixed wrong baudrate calculation method.

[2.1.0]#

  • Bug Fixes

  • Fixed wrong definitions of interrupt enable/disable masks.

  • Fixed wrong usage of QSPI_DisableInterrupts.

  • Fixed wrong type casts.

  • Fixed bug for master blocking transfer of rx FIFO overflow.

[2.0.0]#

  • Initial version.

SIM#

[2.1.0]#

  • Improvements

  • Updated support for MC56F82xxx and MC56F84xxx.

    • Bug Fixes

  • Fixed violations of the MISRA C-2012 rules.

[2.0.0]#

  • Initial version.

DSC_XBARA#

[2.0.2]#

  • Improvements

    • Updated XBARA_SELx_SELn_MASK macro to use SOC register bit field macros (XBARA_SEL0_SEL0_MASK / XBARA_SEL0_SEL1_MASK) instead of hardcoded values.

[2.0.1]#

  • Bug Fixes

  • Fixed violations of the MISRA C-2012 rules.

[2.0.0]#

  • Initial version.

XBARB#

[2.0.0]#

  • Initial version.