Xtensa Audio Framework (XAF) Examples#
Overview#
The Xtensa Audio Framework (XAF) is designed to accelerate the development of audio processing applications for the HiFi family of DSP cores. The multicore version of XAF described in these examples is designed to work with subsystems having single or multiple DSPs, enabling sophisticated audio processing capabilities in embedded systems.
Each demo showcases a dual-core architecture:
cm33/ - The ARM application for the Cortex-M33 core, which provides the user interface and system control
dsp/ - The DSP application that performs audio processing using the XAF middleware library
When an application is started, a shell interface is displayed on the terminal that executes from the ARM core. Users can control the application through shell commands, which are relayed via RPMsg-Lite IPC to the DSP core where they are processed and responses are returned. This architecture demonstrates efficient partitioning of workloads - with user interface and control tasks handled by the ARM core while computationally intensive audio processing is offloaded to the specialized DSP core.
For more information about XAF and detailed documentation on the API and available components, please refer to the Cadence XAF documentation (/middleware/cadence/multicore-xaf/xa_af_hostless/doc).
Availability Note#
Important: These XAF examples are not included in the standard MCUXpresso SDK repository. They are available as part of the MCUXpresso SDK Builder package on the NXP website. To access these examples, please visit MCUXpresso SDK Builder and create a customized SDK package that includes the XAF examples for your target platform.
Included Examples#
XAF Playback Example#
The dsp_xaf_playback application demonstrates audio file decoding and playback capabilities using the DSP core and Xtensa Audio Framework, supporting various audio codecs while handling operations through a shell interface on the ARM core that communicates with DSP processing.
XAF Record Example#
The dsp_xaf_record example captures audio from digital microphones (DMIC), processes it on the DSP core using voice enhancement algorithms, performs voice recognition (VIT), and outputs the detected wake words and voice commands to the console, enabling hands-free voice control applications.
XAF USB Example#
The XAF USB example demonstrates DSP-powered USB audio processing in two configurations: USB speaker and USB microphone. The application uses shell commands to switch between modes, with the ARM core handling USB communication while the DSP processes audio.