MCUXpresso SDK Documentation

MCUXpresso SDK Release Notes#

Development tools#

The MCUXpresso SDK was tested with following development tools. Same versions or above are recommended.

  • IAR Embedded Workbench for Arm, version is 9.70.4

  • MCUXpresso for VS Code v26.06

  • GCC Arm Embedded Toolchain 14.2.x

Supported development systems#

This release supports board and devices listed in following table. The board and devices in bold were tested in this release.

Development boards

MCU devices

MCIMX93-QSB

MIMX9311CVXXM, MIMX9311DVXXM, MIMX9311XVXXM,
MIMX9312CVXXM, MIMX9312DVXXM, MIMX9312XVXXM,
MIMX9321CVXXM, MIMX9321DVXXM, MIMX9321XVXXM,
MIMX9322CVXXM, MIMX9322DVXXM, MIMX9322XVXXM

MCUXpresso SDK release package#

The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.

Device support#

The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.

Board support#

The boards folder provides the board-specific demo applications, driver examples, and middleware examples.

Demo application and other examples#

The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.

RTOS#

FreeRTOS#

Real-time operating system for microcontrollers from Amazon

Middleware#

CMSIS DSP Library#

The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.

VoiceSpot#

VoiceSpot is a highly accurate, small memory and MIPS profile wake word engine supporting custom voice trigger words and phrases. MCUXpresso SDK version of VoiceSpot is trained to “Hey NXP” wake word only and has 25 hour trial timeout.

TinyCBOR#

Concise Binary Object Representation (CBOR) Library

PKCS#11#

The PKCS#11 standard specifies an application programming interface (API), called “Cryptoki,” for devices that hold cryptographic information and perform cryptographic functions. Cryptoki follows a simple object based approach, addressing the goals of technology independence (any kind of device) and resource sharing (multiple applications accessing multiple devices), presenting to applications a common, logical view of the device called a “cryptographic token”.

Multicore#

Multicore Software Development Kit

eIQ#

The package contains several example applications using the eIQ TensorFlow Lite for Microcontrollers library.

eIQ machine learning SDK containing:

  • Arm CMSIS-NN library (neural network kernels optimized for Cortex-M cores)

  • Inference engines:

    • TensorFlow Lite Micro

    • DeepView RT

  • Example code for TensorFlow Lite Micro, Glow, and DeepView RT

lwIP#

The lwIP TCP/IP stack is pre-integrated with MCUXpresso SDK and runs on top of the MCUXpresso SDK Ethernet driver with Ethernet-capable devices/boards.

For details, see the lwIP TCPIP Stack and MCUXpresso SDK Integration User’s Guide (document MCUXSDKLWIPUG).

lwIP is a small independent implementation of the TCP/IP protocol suite.

llhttp#

HTTP parser llhttp

FreeMASTER#

FreeMASTER communication driver for 32-bit platforms.

Release contents#

Provides an overview of the MCUXpresso SDK release package contents and locations.

Deliverable

Location

Boards

INSTALL_DIR/boards

Demo Applications

INSTALL_DIR/boards/<board_name>/demo_apps

Driver Examples

INSTALL_DIR/boards/<board_name>/driver_examples

eIQ examples

INSTALL_DIR/boards/<board_name>/eiq_examples

Board Project Template for MCUXpresso IDE NPW

INSTALL_DIR/boards/<board_name>/project_template

Driver, SoC header files, extension header files and feature header files, utilities

INSTALL_DIR/devices/<device_name>

CMSIS drivers

INSTALL_DIR/devices/<device_name>/cmsis_drivers

Peripheral drivers

INSTALL_DIR/devices/<device_name>/drivers

Toolchain linker files and startup code

INSTALL_DIR/devices/<device_name>/<toolchain_name>

Utilities such as debug console

INSTALL_DIR/devices/<device_name>/utilities

Device Project Template for MCUXpresso IDE NPW

INSTALL_DIR/devices/<device_name>/project_template

CMSIS Arm Cortex-M header files, DSP library source

INSTALL_DIR/CMSIS

Components and board device drivers

INSTALL_DIR/components

RTOS

INSTALL_DIR/rtos

Release Notes, Getting Started Document and other documents

INSTALL_DIR/docs

Tools such as shared cmake files

INSTALL_DIR/tools

Middleware

INSTALL_DIR/middleware

Known Issues#

This section lists the known issues, limitations, and/or workarounds.

eDMA examples accessing AIPS peripheral bridge memory must run through U-Boot loading method#

Non-secure access to Arm IP Bus (AIPS) must be configured in Trusted Resource Domain Control (TRDC) for enhanced direct memory access (eDMA) controller. Due to the limitation that Sentinel ROM can release TRDC only once, such examples must run through U-Boot loading method after Trusted Firmware-A (TF-A) configuring TRDC.

To make low-power boot mode work for only M core in such example, you need to implement the request of the TRDC release and configure TRDC. However, it will break the single boot mode with TF-A/Linux BSP.

The following eDMA examples need access to AIPS.

  • cmsis_lpi2c_edma_b2b_transfer_master

  • cmsis_lpi2c_edma_b2b_transfer_slave

  • cmsis_lpuart_edma_transfer

  • flexcan_loopback_edma_transfer

  • lpi2c_edma_b2b_transfer_master

  • lpi2c_edma_b2b_transfer_slave

  • lpuart_edma_transfer

  • pdm_edma_transfer

  • sai_edma_transfer

Examples hello_world_ns, secure_faults_ns, and secure_faults_trdc_ns have incorrect library path in GUI projects#

When the affected examples are generated as GUI projects, the library linking the secure and non-secure worlds has an incorrect path set. This causes linking errors during project compilation.

Examples: hello_world_ns, hello_world_s, secure_faults_ns, secure_faults_s, secure_faults_trdc_ns, secure_faults_trdc_s

Affected toolchains: mdk, iar

Workaround: In the IDE project settings for the non-secure (_ns) project, find the linked library (named hello_world_s_CMSE_lib.o, or similar, depending on the example project) and replace the path to the library with <build_directory>/<secure_world_project_folder>/<IDE>/, replacing the subdirectory names with the build directory, the secure world project name, and IDE name.