Getting Started with Package# Table of Contents MCUXpresso SDK board support folders Example application structure Locating example application source files Toolchain introduction Compiler/Debugger Run a demo application using IAR Build an example application Run an example application Run a demo using ARMGCC / VSCODE Running an application by U-Boot Program flash.bin to SD/eMMC with UUU Set up environment Download the Universal Upgrade Utility Switch to Download mode Build an example application Run an example application How to determine COM port