MCUXpresso SDK Release Notes#
Development tools#
The MCUXpresso SDK was tested with following development tools. Same versions or above are recommended.
MCUXpresso IDE, Rev. 25.06.xx
IAR Embedded Workbench for Arm, version is 9.70.4
Keil MDK, version is 5.43a
MCUXpresso for VS Code v26.06
GCC Arm Embedded Toolchain 14.2.x
Supported development systems#
This release supports board and devices listed in following table. The board and devices in bold were tested in this release.
Development boards |
MCU devices |
|---|---|
FRDM-MCXA174 |
MCXA173VFM, MCXA173VLF, MCXA173VLH, |
MCUXpresso SDK release package#
The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.
Device support#
The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.
Board support#
The boards folder provides the board-specific demo applications, driver examples, and middleware examples.
Demo application and other examples#
The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.
RTOS#
FreeRTOS#
Real-time operating system for microcontrollers from Amazon
Middleware#
CMSIS DSP Library#
The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.
LittleFS#
LittleFS filesystem stack
Motor Control Software (ACIM, BLDC, PMSM)#
Motor control examples.
FreeMASTER#
FreeMASTER communication driver for 32-bit platforms.
File systemFatfs#
The FatFs file system is integrated with the MCUXpresso SDK and can be used to access either the SD card or the USB memory stick when the SD card driver or the USB Mass Storage Device class implementation is used.
Release contents#
Provides an overview of the MCUXpresso SDK release package contents and locations.
Deliverable |
Location |
|---|---|
Boards |
INSTALL_DIR/boards |
Demo Applications |
INSTALL_DIR/boards/<board_name>/demo_apps |
Driver Examples |
INSTALL_DIR/boards/<board_name>/driver_examples |
eIQ examples |
INSTALL_DIR/boards/<board_name>/eiq_examples |
Board Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/boards/<board_name>/project_template |
Driver, SoC header files, extension header files and feature header files, utilities |
INSTALL_DIR/devices/<device_name> |
CMSIS drivers |
INSTALL_DIR/devices/<device_name>/cmsis_drivers |
Peripheral drivers |
INSTALL_DIR/devices/<device_name>/drivers |
Toolchain linker files and startup code |
INSTALL_DIR/devices/<device_name>/<toolchain_name> |
Utilities such as debug console |
INSTALL_DIR/devices/<device_name>/utilities |
Device Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/devices/<device_name>/project_template |
CMSIS Arm Cortex-M header files, DSP library source |
INSTALL_DIR/CMSIS |
Components and board device drivers |
INSTALL_DIR/components |
RTOS |
INSTALL_DIR/rtos |
Release Notes, Getting Started Document and other documents |
INSTALL_DIR/docs |
Tools such as shared cmake files |
INSTALL_DIR/tools |
Middleware |
INSTALL_DIR/middleware |
Known Issues#
This section lists the known issues, limitations, and/or workarounds.
Cannot add SDK components into FreeRTOS projects#
It is not possible to add any SDK components into FreeRTOS project using the MCUXpresso IDE New Project wizard.