Getting Started with Package# Table of Contents MCUXpresso SDK board support folders Example application structure Locating example application source files Toolchain introduction Compiler/Debugger Run a demo application using IAR Build an example application Run an example application Run a demo using ARMGCC / VSCODE Running an application by U-Boot Run a flash target demo by UUU Set up environment Download the MfgTool Switch to Download Mode Build an example application Run an example application How to determine COM port