MCUXpresso SDK Release Notes for EVK-MIMX8ULP# Table of Contents MCUXpresso SDK board support folders Example application structure Locating example application source files Toolchain introduction Compiler/Debugger Running a Demo Application Using Arm GCC Linux OS host Set up toolchain Install GCC Arm embedded toolchain Add a new system environment variable for ARMGCC_DIR Build an example application Windows OS host Set up toolchain Install GCC Arm embedded toolchain Add a new system environment variable for ARMGCC_DIR Build an example application Running a demo application using IAR Build an example application Run an application using imx-mkimage Memory attribution map after doing handshake How to determine COM port How to set up Windows/Linux host system