Getting Started with Package# Table of Contents MCUXpresso SDK board support package folders Example application structure Locating example application source files Run a demo application using IAR Build an example application Run an example application Run a demo using Keil® MDK/μVision Install CMSIS device pack Build an example application Run an example application Run a demo using ARMGCC / VSCODE Run a demo using MCUXpresso IDE Select the workspace location Build an example application Run an example application How to determine COM port How to define IRQ handler in CPP files How to add or remove boot header for XIP targets