Safety IEC60730B#
Safety is an obligatory part of many applications. It is controlled by international standards related to electrical devices. The affected devices are those that, in case of failure, can cause injury, death, pollution, or other dangerous situations.
Documentation#
The documentation is provided on IEC 60730 Safety Standard for Household Appliances web.
License#
This repository is under LA_OPT_Online Code Hosting NXP_Software_License.
Examples#
Check repository mcux-sdk-examples for specific board and available safety_iec60730b examples. The following application types are available:
safety_iec60730b - This application demonstrates use of certified NXP Safety Library which meets the IEC60730 class B standard.
Setup#
Instructions on how to install the MCUXpresso SDK provided from GitHub via west manifest SDK Installation Instructions or how to evaluate an example project Building Example Projects.