Getting Started with Package# Table of Contents MCUXpresso SDK board support folders Example application structure Locating example application source files Toolchain introduction Compiler/Debugger Build a demo application using Arm GCC Linux OS host Set up toolchain Install GCC Arm embedded toolchain Add a new system environment variable for ARMGCC_DIR Build an example application Windows OS host Set up toolchain Install GCC Arm embedded toolchain Add a new system environment variable for ARMGCC_DIR Build an example application Build a demo application with IAR Build an example application Generate a flash.bin Enable MCU UARTs Run a demo application Run an example application Generate a flash.bin Debug an demo application with IAR How to determine COM port Host setup