MCUXpresso SDK Documentation

Wireless connectivity middleware overview#

Component versions:

Wireless connectivity component

Version

middleware/​wireless/​bluetooth

1.10.14

middleware/​wireless/​ble_​controller

1.9.37.0

middleware/wireless/ieee-802.15.4

1.0.21b

middleware/​wireless/​xcvr

​2.​1.4

middleware/​wireless/​genfsk

4.0.22

middleware/wireless/framework

7.0.1b

middleware/wireless/zigbee

1.0.16b

The following connectivity-supporting documentation is included with this release:

  • Bluetooth Low Energy Quick Start Guide

  • Bluetooth Low Energy Demo Applications User’s Guide

  • Bluetooth Low Energy Application Developer’s Guide

  • Bluetooth Low Energy Host Stack API Reference Manual

  • Bluetooth Low Energy Host Stack FSCI Application Programming

  • Bluetooth Low Energy Host Stack FSCI Reference Manual

  • Bluetooth Low Energy Connection Handover

  • Bluetooth Low Energy Localization Application Note

  • Bluetooth Low Energy Channel Sounding Application Developers Guide

  • Bluetooth Channel Sounding Technique for Distance Estimation

  • CS Wireless Ranging Demo Application User Guide

  • Generic FSK Link Layer Quick Start Guide

  • Generic FSK Link Layer API Reference Manual

  • Connectivity Framework Reference Manual

  • Connectivity Framework API Documentation

  • Low Power Connectivity Reference Design User’s Guide

  • Zigbee Demo Applications User Guide

  • ZigBee 3.0 Stack User Guide

  • ZigBee Cluster Library User Guide

  • ZigBee 3.0 Devices User Guide

  • Zigbee Green Power User Guide

  • Zigbee Core Utilities User Guide

  • IEEE 802.15.4 Connectivity Test Application Getting Started Guide

  • IEEE 802.15.4 Connectivity Test Application Command Line Interface User Guide

Bluetooth LE Host Stack and Applications#

The Bluetooth LE Host Stack component provides an implementation for a Bluetooth 6.0 mandatory and some optional, proprietary, and experimental features. The Bluetooth LE Host Stack component provides application examples, services, and profiles.

Main features supported:

  • Automotive Compliance

  • MISRA Compliance

  • HIS CCM <= 20

  • Advanced Secure Mode

  • Enhanced ATT

  • GATT Caching

  • GCC Libraries

  • IAR Libraries

  • Bluetooth LE Peripheral Libraries

  • Bluetooth LE Central Libraries

  • Bluetooth LE Full Host Features Libraries

  • Bluetooth LE Host Optional Features Libraries

  • Bluetooth LE Host Mandatory Features Libraries

  • BareMetal and FreeRTOS Support

  • Full Privacy Support

  • NCP Mode - FSCI Application

  • Enhanced Notifications

  • Dynamic Database

  • OTA Support - Sample Applications

  • Decision based Advertising Filtering (DBAF)

  • Advertising Coding Selection (ACS)

  • Periodic Advertising with Responses (PAwR)

  • Encrypted Advertising Data (EAD)

  • Monitoring Advertisers - Experimental feature

  • Randomized RPA - Experimental feature

  • LE Enhanced Connection Update - Experimental feature

  • Intrusion Detection System (IDS)

    Note: The CDE (Complex-domain Distance Estimation) algorithm is an experimental feature intended only for testing purposes. It is not maintained and must not be included in the production environments.

    Parent topic:Wireless connectivity middleware overview

Bluetooth LE Controller#

Refer to the Bluetooth LE Controller release notes in the middleware documentation.

IEEE 802.15.4#

Refer to the IEEE 802.15.4 release notes in the middleware documentation.

XCVR#

Refer to the XCVR release notes in the middleware documentation.

Low Power Reference Design Applications#

Refer to the Low Power Reference Design release notes in the middleware documentation.

Zigbee#

Refer to the Zigbee release notes in the middleware documentation.

Connectivity Framework#

Refer to the Connectivity Framework release notes in the middleware documentation.

Parent topic:Middleware