MCUXpresso SDK Documentation

Run a demo using ARMGCC / VSCODE

Run a demo using ARMGCC / VSCODE#

This section describes the steps to run an example application from the SDK archive using the ARMGCC / VSCODE toolchain.

Only the J‑Link debugging interface is supported when using JLinkGDBServer and GDB.

Refer to the running a demo using MCUXpresso VSC section for detailed instructions on setting up and configuring your project in Visual Studio Code.

Refer to the CLI section for detailed instructions on building and running your project from the command line.