MCUXpresso SDK Documentation

Boot or Run from Flash

Boot or Run from Flash#

Boot from Flash is straight forward when using IAR environment. SDK provides either two or four different build configurations based on the project: debug (from SRAM)/ release (from SRAM)/ flash_debug/ flash_release. Flash configurations use different memory map in project linker options. For details, see Figure 1.

To enable booting from flash, change the ISP mode/ SW5 switches on the EVK.

If using MCUXpresso/ armgcc build environment, note that by default build environment is set to boot from flash. Using MCUXpresso as an example:

  1. Make sure to use the latest version of MCUXpresso.

  2. Import the SDK examples.

  3. Once completed, double click the last file/ J-Link Debug.

  4. Launch to modify J-Link debugger setting.

  5. Make sure to deselect Reset before running. This helps the flash-based program get into main function.

  • Make sure to:

    • Modify DSP_IMAGE_COPY_TO_RAM and Define to 1 in Project settings > C/C++ General > Paths and Symbols > Symbols.

    • Have the right compilation flag as C/C++. Compilation flags do not work on *.S files.

    • Have #define DSP_IMAGE_COPY_TO_RAM 1 as the first line of source/incbin.S to include the DSP binaries.

    • Use the correct DSP binaries at correct path (must be release binaries).

    • Provide the right image path to incbin.S.

  • To run/boot from flash, make sure that the board is set to FlexSPI flash boot mode (ISP2: ISP1: ISP0 = ON, OFF, ON).

Parent topic:HiFi4 Boot Loader and Memory Map