Hardware requirements
Micro USB cable
MIMXRT1024-EVK board
Adafruit TFT LCD shield w/Cap Touch
Personal Computer
Board settings
There are different versions of Adafruit 2.8” TFT LCD shields. The shields marked v2.0 works directly with this project. For the other shields, please solder the center pin of IOREF pads to the 3.3V pad, and solder the pads 11, 12, and 13. See the link for details: https://community.nxp.com/t5/MCUXpresso-Community-Articles/Modifying-the-latest-Adafruit-2-8-quot-LCD-for-SDK-graphics/ba-p/1131104
Attach the LCD shield to the board.
Prepare the Demo
Connect a micro USB cable between the PC host and the J23 micro USB port on the board.
Build the project.
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
If this example runs correctly, the sample GUI is displayed. Known issue: The MCU is not able to generate hardware reset of the LCD due to hardware limitation of the boards interconnection. Because of this the LCD may not get initialized (stays blank) following a cold start (power on) of the board even if the demo was correctly programmed to the FLASH memory. In such a case simply press the reset button to restart the demo.