MCUXpresso SDK Documentation

This file contains the general information which can be shared by the examples on this board. The example specific information can be found in readme.md or example_board_readme.md.

General Example Settings#

Hardware requirements#

  • Type-C USB cable

  • FRDM-IMXRT700 board

  • Personal Computer

  • 5V external power supply(When display or/and WiFi module are used)

Prepare the Demo#

  1. Connect a USB cable between the PC host and the USB port on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Project Configuration#

SDK project supports two kinds of configure methods:

  1. Configure by Kconfig, passing configuration flags during build: west build ....

  2. OR configure by modifing the macros in configure file mcux_config.h.

NOTE: The mcux_config.h is generated by Kconfig, if Kconfig is used, don’t modify mcux_config.h directly, because the manual changes will be overwritten by Kconfig. NOTE: When the macros to be modified don’t exist in the mcux_config.h, add them directly in mcux_config.h.

Display settings#

This board supports such panels:

  • RaspberryPi Panel

This section describes the general display related settings. Some projects may have special display settings, such as LVGL project. Please refer LVGL project lv_examples_readme.md for the steps.

Board hardware settings#

NOTE: An external 5V power supply is required when using the Raspberry panel. Connect the 5V supply to the board’s external power input and connect J2 1-2.

  • Raspberry panel

    • Connect the panel to J8

    • Connect the panel’s 5V pin to JP43-1, GND pin to JP43-2.

Steps to select the panel#

Please read section Project Configuration to know the configuration methods first.

Panel configuration#

Please read section Project Configuration to know the configuration methods first.

RaspberryPi#

Pixel format#

  • Only RGB565 is supported