Hardware requirements#
Type-C USB cable
FRDM-MCXW72 Board
Personal Computer
Board settings#
No special is needed.
Prepare the Demo#
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
VREF example
ADC Full Range: 65536
Default (Factory) trim value is :15
Use trim value: 0
ADC conversion result: 19861
Actual voltage on VREF_OUT: 1.000V
Use trim value: 1
ADC conversion result: 21827
Actual voltage on VREF_OUT: 1.099V
Use trim value: 2
ADC conversion result: 23812
Actual voltage on VREF_OUT: 1.199V
Use trim value: 3
ADC conversion result: 25792
Actual voltage on VREF_OUT: 1.299V
Use trim value: 4
ADC conversion result: 27776
Actual voltage on VREF_OUT: 1.399V
Use trim value: 5
ADC conversion result: 29741
Actual voltage on VREF_OUT: 1.498V
Use trim value: 6
ADC conversion result: 31790
Actual voltage on VREF_OUT: 1.601V
Use trim value: 7
ADC conversion result: 33734
Actual voltage on VREF_OUT: 1.699V
Use trim value: 8
ADC conversion result: 35763
Actual voltage on VREF_OUT: 1.801V
Use trim value: 9
ADC conversion result: 37699
Actual voltage on VREF_OUT: 1.898V
Use trim value: 10
ADC conversion result: 39667
Actual voltage on VREF_OUT: 1.997V
Use trim value: 11
ADC conversion result: 41632
Actual voltage on VREF_OUT: 2.096V