MCUXpresso SDK Documentation

Hardware requirements#

  • Mini USB cable

  • TWR-MC56F8200 board

  • Personal Computer

  • Oscilloscope

Board hardware common setting#

  1. HW reworkd(workaround):

    Connect J18(the mini USB port) pin4 and pin5. Note: This is due to HW design error, correct setting should be: J18 pin4 left empty and pin5 connected GND.

  2. Power setting:

    Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2

  3. UART setting:

    Connect J8 pin3 and pin4 Connect J9 pin3 and pin4

  4. Onboard OSJTAG debugger setting:

    Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open

Board settings#

  • Use oscilloscope to monitor J501-19.

Prepare the Demo#

  1. Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

When the demo runs successfully, the following message is displayed in the terminal:


****Output PWM example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~