Hardware requirements#
Mini USB cable
TWR-MC56F8400 board
Personal Computer
Oscilloscope
Board hardware common setting#
Power setting:
Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2
UART setting:
Connect J8 pin3 and pin4 Connect J9 pin3 and pin4
Onboard OSJTAG debugger setting:
Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open
Board settings#
Use oscilloscope to monitor J503-29.
Prepare the Demo#
Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board with OSJTAG debug configuration.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
When the demo runs successfully, the following message is displayed in the terminal:
****Output PWM example.****
*********Make sure to connect an oscilloscope.*********
****A 50 duty cycle PWM wave is observed on an oscilloscope.****
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~