MCUXpresso SDK Documentation

cmsis_lpspi_edma_b2b_transfer_slave

cmsis_lpspi_edma_b2b_transfer_slave#

Overview#

The cmsis_lpspi_edma_b2b_transfer example shows how to use LPSPI CMSIS driver with eDMA.

In this example, we need two boards, one board used as LPSPI master and another board used as LPSPI slave. The file ‘cmsis_lpspi_edma_b2b_transfer_slave.c’ includes the LPSPI slave code.

The LPSPI master send/receive data to/from LPSPI slave using eDMA.

Running the demo#

When the demo runs successfully, you will see output in the terminal like this:

LPSPI CMSIS driver board to board edma example.

Slave example is running...

This is LPSPI_SlaveSignalEvent_t
Slave receive data from master has completed!
This is LPSPI_SlaveSignalEvent_t
Slave transmit data to master has completed!

Slave received:
     1  2  3  4  5  6  7  8  9  A  B  C  D  E  F 10
    11 12 13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F 20
    21 22 23 24 25 26 27 28 29 2A 2B 2C 2D 2E 2F 30
    31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F 40

Slave example is running...

Supported Boards#

EVK9-MIMX8ULP
Hardware requirements
  • Micro USB cable

  • two MIMX8ULP-EVK/EVK9 boards

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

Board settings

Remove R139, R159 and populate R140, R158 on both base boards.

SPI one board: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board

INSTANCE0(SPI1)     CONNECTS TO         INSTANCE0(SPI1)
Pin Name   Board Location     Pin Name  Board Location
SPI1_SCK    J23 pin 4            SPI1_SCK  J23 pin 4
SPI1_SIN    J23 pin 2            SPI1_SOUT J23 pin 3
SPI1_SOUT   J23 pin 3            SPI1_SIN  J23 pin 2
SPI1_PCS0   J23 pin 1            SPI1_PCS0 J23 pin 1
GND                             GND
Prepare the Demo
  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.

  2. Connect a micro USB cable between the host PC and the J17 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.

IMX952LPD5EVK-19
Hardware requirements
  • Micro USB cable

  • two IMX952-EVK boards

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

set SW1 into 0000 on IMX952-EVK

Transfer data from one board instance to another board’s instance. SPI7 pins are connected with SPI7 pins of another board

INSTANCE0(SPI7)     CONNECTS TO         INSTANCE0(SPI7)
Pin Name   Board Location       Pin Name  Board Location
SPI_SCK    IMX952LPD5EVK-19   JP1   pin 5	  SPI7_SCK  IMX952LPD5EVK-19    JP1 pin 5
SPI_SIN    IMX952LPD5EVK-19   JP1   pin 3          SPI7_SOUT IMX952LPD5EVK-19    JP1 pin 4
SPI_SOUT   IMX952LPD5EVK-19   JP1   pin 4          SPI7_SIN  IMX952LPD5EVK-19    JP1 pin 3
SPI_PCS0   IMX952LPD5EVK-19   JP1   pin 2          SPI7_PCS0 IMX952LPD5EVK-19    JP1 pin 2
GND                             GND
Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.

EVKB-IMXRT1050
Hardware requirements
  • Mini/micro USB cable

  • EVKB-IMXRT1050 board

  • Personal Computer

Board settings

Remove the resistor R334 and weld 0Ω resistor to R278,R279,R280,R281.

LPSPI:

INSTANCE1(LPSPI1)     CONNECTS TO         INSTANCE1(LPSPI1)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J24 pin 4           SIN       J24 pin 5
SIN         J24 pin 5           SOUT      J24 pin 4
SCK         J24 pin 6           SCK       J24 pin 6
PCS0        J24 pin 3           PCS0      J24 pin 3 
GND         J24 pin 7           GND       J24 pin 7
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MIMXRT1060-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKB board

  • Personal Computer

Board settings

Weld 0Ω resistor to R346,R350,R356,R362.

LPSPI:

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J17-4                SIN       J17-5
SIN        J17-5                SOUT      J17-4
SCK        J17-6                SCK       J17-6
PCS0       J17-3                PCS0      J17-3
GND        J17-7                GND       J17-7
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MIMXRT1170-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Personal Computer

Board settings

Remove 0Ω resistors R200,R404,R406.

LPSPI:

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J10-8                SIN       J10-10
SIN        J10-10               SOUT      J10-8
SCK        J10-12               SCK       J10-12
PCS0       J10-6                PCS0      J10-6
GND        J10-14               GND       J10-14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MIMXRT1060-EVKC
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKC board

  • Personal Computer

Board settings

Weld 0Ω resistor to R346,R350,R356,R362.

LPSPI:

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J17-4                SIN       J17-5
SIN        J17-5                SOUT      J17-4
SCK        J17-6                SCK       J17-6
PCS0       J17-3                PCS0      J17-3
GND        J17-7                GND       J17-7
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-IMXRT1152
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1152 board

  • Personal Computer

Board settings

LPSPI:

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT        J11 pin 8           SIN       J11 pin 10
SIN         J11 pin 10          SOUT      J11 pin 8
SCK         J11 pin 12          SCK       J11 pin 12
PCS0        J11 pin 6           PCS0      J11 pin 6 
GND         J11 pin 14          GND       J11 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

EVK-MCIMX7ULP
Hardware requirements
  • Micro USB cable

  • two MCIMX7ULP-EVK boards

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

Board settings

Populate R188, R189, R190, R191 on both base boards.

SPI one board: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board

INSTANCE0(SPI1)     CONNECTS TO         INSTANCE0(SPI1)
Pin Name   Board Location     Pin Name  Board Location
SPI1_SCK    J8 pin 6            SPI1_SCK  J8 pin 6
SPI1_SIN    J8 pin 5            SPI1_SOUT J8 pin 4
SPI1_SOUT   J8 pin 4            SPI1_SIN  J8 pin 5
SPI1_PCS0   J8 pin 3            SPI1_PCS0 J8 pin 3
GND                             GND

Please note this application can’t support running with Linux BSP! Note

Because of the LPSPI signal pin allocating issue, you can not restart this demo/example by press the ResetButton(SW3):
The LPSPI1_SIN, LPSPI1_SOUT, LPSPI1_SCK and LPSPI1_PCS0 pins are connected to PTA12, PTA13, PTA14 and PTA15 pads.
These pins are also used as BOO_CFG12, BOO_CFG13, BOO_CFG14 and BOO_CFG15 when the i.MX SoC reboot. These signals are
driven by LPSPI1 pins on the other board, when user press ResetButton. This may cause M4 Core enter enter
incorrect boot modes and only re-powerup both boards can let the M4 core exit such modes.

##### Prepare the Demo
1.  Connect 5V power supply and J-Link Debug Probe to the board, switch SW1 to power on the board.
2.  Connect a micro USB cable between the host PC and the J6 USB port on the target board.
3.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
4.  Download the program to the target board.
5.  Either cold boot your board or launch the debugger in your IDE to begin running the example.
EVK-MIMX8ULP
Hardware requirements
  • Micro USB cable

  • two MIMX8ULP-EVK/EVK9 boards

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

Board settings

Remove R139, R159 and populate R140, R158 on both base boards.

SPI one board: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board

INSTANCE0(SPI1)     CONNECTS TO         INSTANCE0(SPI1)
Pin Name   Board Location     Pin Name  Board Location
SPI1_SCK    J23 pin 4            SPI1_SCK  J23 pin 4
SPI1_SIN    J23 pin 2            SPI1_SOUT J23 pin 3
SPI1_SOUT   J23 pin 3            SPI1_SIN  J23 pin 2
SPI1_PCS0   J23 pin 1            SPI1_PCS0 J23 pin 1
GND                             GND
Prepare the Demo
  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.

  2. Connect a micro USB cable between the host PC and the J17 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.

EVK-MIMXRT1010
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1010 board

  • Personal Computer

Board settings

LPSPI:

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J57-10                SIN       J57-8
SIN        J57-8                 SOUT      J57-10
SCK        J57-12                SCK       J57-12
PCS0       J57-6                 PCS0      J57-6
GND        J57-14                GND       J57-14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

EVK-MIMXRT1015
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1015 board

  • Personal Computer

Board settings

Remove R293 LPSPI:

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J19-4                SIN       J19-5
SIN        J19-5                SOUT      J19-4
SCK        J19-6                SCK       J19-6
PCS0       J19-3                PCS0      J19-3
GND        J19-7                GND       J19-7
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

EVK-MIMXRT1020
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1020 board

  • Personal Computer

Board settings

LPSPI:

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J19-4                SIN       J19-5
SIN        J19-5                SOUT      J19-4
SCK        J19-6                SCK       J19-6
PCS0       J19-3                PCS0      J19-3
GND        J19-7                GND       J19-7
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

MIMXRT1024-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1024-EVK board

  • Personal Computer

Board settings

LPSPI:

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J19-8                SIN       J19-10
SIN        J19-10               SOUT      J19-8
SCK        J19-12               SCK       J19-12
PCS0       J19-6                PCS0      J19-6
GND        J19-14               GND       J19-14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

MIMXRT1040-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1040-EVK board

  • Personal Computer

Board settings

Weld 0Ω resistor to R346,R350,R356,R362.

LPSPI:

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J17-4                SIN       J17-5
SIN        J17-5                SOUT      J17-4
SCK        J17-6                SCK       J17-6
PCS0       J17-3                PCS0      J17-3
GND        J17-7                GND       J17-7
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

EVK-MIMXRT1064
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1064 board

  • Personal Computer

Board settings

Weld 0Ω resistor to R278,R279,R280,R281.

LPSPI:

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J24-4                SIN       J24-5
SIN        J24-5                SOUT      J24-4
SCK        J24-6                SCK       J24-6
PCS0       J24-3                PCS0      J24-3
GND        J24-7                GND       J24-7
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MIMXRT1160-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1160-EVK board

  • Personal Computer

Board settings

Remove 0Ω resistors R200,R404,R406,R408.

LPSPI:

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J10-8                SIN       J10-10
SIN        J10-10               SOUT      J10-8
SCK        J10-12               SCK       J10-12
PCS0       J10-6                PCS0      J10-6
GND        J10-14               GND       J10-14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MIMXRT1180-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1180-EVK board

  • Personal Computer

Board settings

SPI one board: Transfer data from one board instance to another board’s instance. SPI3 pins are connected with SPI3 pins of another board

INSTANCE(LPSPI3)     CONNECTS TO    INSTANCE(LPSPI3)
Pin Name   Board Location   Pin Name   Board Location
SOUT       J44-8            SIN        J44-10
SIN        J44-10           SOUT       J44-8
SCK        J44-12           SCK        J44-12
PCS0       J44-6            PCS0       J44-6 
GND        J44-14           GND        J44-14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-K32L2A4S
Hardware requirements
  • Mini USB cable

  • Two FRDM-K32L2A4S boards

  • Personal Computer

Board settings

SPI one board: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board

INSTANCE0(SPI0)     CONNECTS TO         INSTANCE0(SPI0)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J2 pin 8            SIN       J2 pin 10
SIN         J2 pin 10           SOUT      J2 pin 8
SCK         J2 pin 12           SCK       J2 pin 12
PCS0        J2 pin 6            PCS0      J2 pin 6
GND         J2 pin 14           GND       J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-K32L3A6
Hardware requirements
  • Mini USB cable

  • Two FRDM-K32L3A6 boards

  • Personal Computer

Board settings

SPI two board: Transfer data from one board instance to another board’s instance. To make lpspi example work(M4), connections needed to be as follows: SPI0 pins are connected with SPI0 pins of another board

INSTANCE0(SPI0)     CONNECTS TO         INSTANCE0(SPI0)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J2 pin 8            SIN       J2 pin 10
SIN         J2 pin 10           SOUT      J2 pin 8
SCK         J2 pin 12           SCK       J2 pin 12
PCS2        J2 pin 6            PCS2      J2 pin 6
GND         J2 pin 14           GND       J2 pin 14

To make lpspi example work(M0), connections needed to be as follows: SPI3 pins are connected with SPI3 pins of another board

INSTANCE3(SPI3)     CONNECTS TO         INSTANCE3(SPI3)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J1 pin 2            SIN       J1 pin 6
SIN         J1 pin 6            SOUT      J1 pin 2
SCK         J3 pin 5            SCK       J3 pin 5
PCS1        J3 pin 9            PCS1      J3 pin 9
GND         J2 pin 14           GND       J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-KE15Z
Hardware requirements
  • Micro USB cable

  • Two FRDM-KE15Z boards

  • Personal Computer

Board settings

SPI one board: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board

INSTANCE0(SPI0)     CONNECTS TO         INSTANCE0(SPI0)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J2 pin 8            SIN       J2 pin 10
SIN         J2 pin 10           SOUT      J2 pin 8
SCK         J2 pin 12           SCK       J2 pin 12
PCS3        J2 pin 6            PCS3      J2 pin 6
GND         J2 pin 14           GND       J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-KE17Z
Hardware requirements
  • Micro USB cable

  • Two FRDM-KE17Z boards

  • Personal Computer

Board settings

SPI two boards: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board

INSTANCE0(SPI0)     CONNECTS TO         INSTANCE0(SPI0)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J2 pin 8            SIN       J2 pin 10
SIN         J2 pin 10           SOUT      J2 pin 8
SCK         J2 pin 12           SCK       J2 pin 12
PCS1        J2 pin 6            PCS1      J2 pin 6
GND         J2 pin 14           GND       J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-KE17Z512
Hardware requirements
  • Micro USB cable

  • Two FRDM-KE17Z512 boards

  • Personal Computer

Board settings

SPI two boards: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board

INSTANCE0(SPI0)     CONNECTS TO         INSTANCE0(SPI0)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J2 pin 8            SIN       J2 pin 10
SIN         J2 pin 10           SOUT      J2 pin 8
SCK         J2 pin 12           SCK       J2 pin 12
PCS1        J2 pin 6            PCS1      J2 pin 6
GND         J2 pin 14           GND       J2 pin 14
Prepare the Demo
  1. Connect a USB cable between the PC host and the MCU-LINK USB port on the board.

  2. Open a serial terminal on PC for MCU-LINK serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-MCXA153
Toolchain supported
  • IAR embedded Workbench 9.40.1

  • Keil MDK 5.38.1

  • GCC ARM Embedded 12.2

  • MCUXpresso 11.8.0

Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA153 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI0)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J6-6                SIN       J2-10
SIN        J6-5                SOUT      J2-8
SCK        J6-4                SCK       J2-12
PCS0       J6-3                PCS1      J2-6
GND        J6-8                GND       J6-8
Prepare the Demo
  1. Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA156
Toolchain supported
  • IAR embedded Workbench 9.40.1

  • Keil MDK 5.38.1

  • GCC ARM Embedded 12.2

  • MCUXpresso 11.8.0

Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA156 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI0)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J6-6                SIN       J3-9
SIN        J6-5                SOUT      J3-11
SCK        J6-4                SCK       J3-7
PCS0       J6-3                PCS1      J3-5
GND        J6-8                GND       J6-8
Prepare the Demo
  1. Connect a Type-C USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA174
Toolchain supported
  • IAR embedded Workbench 9.40.1

  • Keil MDK 5.38.1

  • GCC ARM Embedded 12.2

  • MCUXpresso 11.8.0

Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA174 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a Type-C USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA344
Toolchain supported
  • IAR embedded Workbench 9.40.1

  • Keil MDK 5.38.1

  • GCC ARM Embedded 12.2

  • MCUXpresso 11.8.0

Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA344 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a Type-C USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA346
Toolchain supported
  • IAR embedded Workbench 9.40.1

  • Keil MDK 5.38.1

  • GCC ARM Embedded 12.2

  • MCUXpresso 11.8.0

Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA346 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a Type-C USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXE247
Hardware requirements
  • USB-C cable

  • Two FRDM-MCXE247 boards

  • Personal Computer

Board settings

SPI two boards: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board

INSTANCE0(SPI0)     CONNECTS TO         INSTANCE0(SPI0)
Pin Name   Board Location     Pin Name  Board Location
SOUT        J6 pin 6            SIN       J6 pin 5
SIN         J6 pin 5            SOUT      J6 pin 6
SCK         J6 pin 4            SCK       J6 pin 4
PCS2        J6 pin 3            PCS2      J6 pin 3
GND         J6 pin 8            GND       J6 pin 8
Prepare the Demo
  1. Connect a USB cable between the PC host and the MCU-LINK USB port on the board.

  2. Open a serial terminal on PC for MCU-LINK serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-MCXL255
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXL255 board

  • Personal Computer

Board settings

LPSPI:

MASTER (SPI1)                       SLAVE (SPI1)
Pin Name        Board Location      Pin Name        Board Location
SOUT            J2-8                SIN             J2-10
SIN             J2-10               SOUT            J2-8
SCK             J2-12               SCK             J2-12
PCS0            J2-6                PCS1            J2-6
GND             J2-14               GND             J2-14

Make sure you have solder bridges SJ1 and SJ2 set to

  • 2-1 for the main core (cm33)

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a Type-C USB cable between the host PC and the MCU-Link port(J16) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXN236
Hardware requirements
  • Mini USB cable

  • FRDM-MCXN236 board

  • Personal Computer

Board settings

LPSPI:

	MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2 Pin 8           SIN         J2 Pin 10
SIN        J2 Pin 10          SOUT        J2 Pin 8
SCK        J2 Pin 12          SCK         J2 Pin 12
PCS0       J2 Pin 6           PCS0        J2 Pin 6
GND        J2 pin 14          GND         J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-MCXN947
Hardware requirements
  • Mini USB cable

  • Two FRDM-MCXN947 boards

  • Personal Computer

Board settings

LPSPI:

	MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2 Pin 8           SIN         J2 Pin 10
SIN        J2 Pin 10          SOUT        J2 Pin 8
SCK        J2 Pin 12          SCK         J2 Pin 12
PCS0       J2 Pin 6           PCS0        J2 Pin 6
GND        J2 pin 14          GND         J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-MCXN947T
Hardware requirements
  • Mini USB cable

  • Two FRDM-MCXN947T boards

  • Personal Computer

Board settings

LPSPI:

	MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2 Pin 8           SIN         J2 Pin 10
SIN        J2 Pin 10          SOUT        J2 Pin 8
SCK        J2 Pin 12          SCK         J2 Pin 12
PCS0       J2 Pin 6           PCS0        J2 Pin 6
GND        J2 pin 14          GND         J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

FRDM-MCXW71
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW71 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Be sure to disconnect the 12V adapter on J9, otherwise the transmission will fail. Jumper setting:

MASTER(SPI0)                connect to      SLAVE(SPI0)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J2 pin 9                         SIN         J1 pin 2
SIN        J1 pin 2                         SOUT        J2 pin 9
SCK        J1 pin 5                         SCK         J1 pin 5
PCS0       J1 pin 1                         PCS0        J1 pin 1

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MCX-W71-EVK
Hardware requirements
  • Type-C USB cable

  • MCX-W71-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Be sure to disconnect the 12V adapter on J9, otherwise the transmission will fail. Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J2 pin 13                        SIN         J2 pin 11
SIN        J2 pin 11                        SOUT        J2 pin 13
SCK        J2 pin 9                         SCK         J2 pin 9
PCS0       J2 pin 15                        PCS0        J2 pin 15

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

KW45B41Z-EVK
Hardware requirements
  • Mini/micro USB cable

  • KW45B41Z-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Be sure to disconnect the 12V adapter on J9, otherwise the transmission will fail. Jumper setting:

MASTER(SPI0)                connect to      SLAVE(SPI0)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J2 pin 2                         SIN         J1 pin 2
SIN        J1 pin 2                         SOUT        J2 pin 2
SCK        J1 pin 5                         SCK         J1 pin 5
PCS0       J1 pin 1                         PCS0        J1 pin 1

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

KW47-EVK
Hardware requirements
  • Type-C USB cable

  • KW47-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Be sure to disconnect the 12V adapter on J9, otherwise the transmission will fail. Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J2 pin 13                        SIN         J2 pin 11
SIN        J2 pin 11                        SOUT        J2 pin 13
SCK        J2 pin 9                         SCK         J2 pin 9
PCS0       J2 pin 15                        PCS0        J2 pin 15

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MCX-N5XX-EVK
Hardware requirements
  • Mini USB cable

  • Two MCX-N5XX-EVK boards

  • Personal Computer

Board settings

LPSPI:

	MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2 Pin 8           SIN         J2 Pin 10
SIN        J2 Pin 10          SOUT        J2 Pin 8
SCK        J2 Pin 12          SCK         J2 Pin 12
PCS0       J2 Pin 6           PCS0        J2 Pin 6
GND        J2 pin 14          GND         J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

MCX-N9XX-EVK
Hardware requirements
  • Mini USB cable

  • Two MCX-N9XX-EVK boards

  • Personal Computer

Board settings

LPSPI:

	MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2 Pin 8           SIN         J2 Pin 10
SIN        J2 Pin 10          SOUT        J2 Pin 8
SCK        J2 Pin 12          SCK         J2 Pin 12
PCS0       J2 Pin 6           PCS0        J2 Pin 6
GND        J2 pin 14          GND         J2 pin 14
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

MCX-W72-EVK
Hardware requirements
  • Type-C USB cable

  • MCX-W72-EVK Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Be sure to disconnect the 12V adapter on J9, otherwise the transmission will fail. Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J2 pin 13                        SIN         J2 pin 11
SIN        J2 pin 11                        SOUT        J2 pin 13
SCK        J2 pin 9                         SCK         J2 pin 9
PCS0       J2 pin 15                        PCS0        J2 pin 15

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MIMXRT700-EVK
Hardware requirements
  • Mini USB cable

  • MIMXRT700-EVK board

  • Personal Computer

Board settings

  1. Make sure JP12 is installed

  2. SPI two boards: Transfer data from one board instance to another board’s instance. SPI14 pins are connected with SPI14 pins of another board

INSTANCE0(SPI14)     CONNECTS TO         INSTANCE0(SPI14)
Pin Name   Board Location           Pin Name  Board Location
SOUT        J20 pin 3                   SIN       J20 pin 5
SIN         J20 pin 5                   SOUT      J20 pin 3
SCK         J20 pin 7                   SCK       J20 pin 7
PCS0        J20 pin 1                   PCS0      J20 pin 1
GND         J20 pin 9                   GND       J20 pin 9
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

KW47-LOC
Hardware requirements
  • Type-C USB cable

  • KW47-LOC Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Be sure to disconnect the 12V adapter on J9, otherwise the transmission will fail. Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J1 pin 6                         SIN         J1 pin 5
SIN        J1 pin 5                         SOUT        J1 pin 6
SCK        J1 pin 4                         SCK         J1 pin 4
PCS0       J1 pin 3                         PCS0        J1 pin 3

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MCXW72-LOC
Hardware requirements
  • Type-C USB cable

  • MCXW72-LOC Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Note: Be sure to disconnect the 12V adapter on J9, otherwise the transmission will fail. Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J1 pin 6                         SIN         J1 pin 5
SIN        J1 pin 5                         SOUT        J1 pin 6
SCK        J1 pin 4                         SCK         J1 pin 4
PCS0       J1 pin 3                         PCS0        J1 pin 3

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-IMXRT1186
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1186 board

  • Personal Computer

Board settings

SPI one board: Transfer data from one board instance to another board’s instance. SPI2 pins are connected with SPI2 pins of another board

INSTANCE(LPSPI2)     CONNECTS TO    INSTANCE(LPSPI2)
Pin Name   Board Location   Pin Name   Board Location
SOUT       J3-16           SIN        J3-14
SIN        J3-14           SOUT       J3-16
SCK        J3-18           SCK        J3-18
PCS0       J3-12           PCS0       J3-12
GND        J2-19           GND        J2-19
Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA266
Toolchain supported
  • IAR embedded Workbench 9.40.1

  • Keil MDK 5.38.1

  • GCC ARM Embedded 12.2

  • MCUXpresso 11.8.0

Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA266 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a Type-C USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA366
Toolchain supported
  • IAR embedded Workbench 9.40.1

  • Keil MDK 5.38.1

  • GCC ARM Embedded 12.2

  • MCUXpresso 11.8.0

Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA366 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a Type-C USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXW72
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW72 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J6 pin 6                         SIN         J6 pin 5
SIN        J6 pin 5                         SOUT        J6 pin 6
SCK        J6 pin 4                         SCK         J6 pin 4
PCS0       J6 pin 3                         PCS0        J6 pin 3

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA577
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA577 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a Type-C USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXC162
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXC162 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI0)      connect to        SLAVE(SPI0)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a Type-C USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-KW43
Hardware requirements
  • Type-C USB cable

  • FRDM-KW43 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J19 pin 5                        SIN         J19 pin 4
SIN        J19 pin 4                        SOUT        J19 pin 5
SCK        J19 pin 6                        SCK         J19 pin 6
PCS0       J19 pin 3                        PCS0        J19 pin 3

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a Type-C USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXW70
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW70 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Jumper setting:

MASTER(SPI1)                connect to      SLAVE(SPI1)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J19 pin 5                        SIN         J19 pin 4
SIN        J19 pin 4                        SOUT        J19 pin 5
SCK        J19 pin 6                        SCK         J19 pin 6
PCS0       J19 pin 3                        PCS0        J19 pin 3

Other jumpers keep default configuration.

Prepare the Demo
  1. Connect a Type-C USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXA287
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA287 board

  • Personal Computer

Board settings

LPSPI:

       MASTER(SPI1)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J2-8               SIN         J2-10
SIN        J2-10              SOUT        J2-8
SCK        J2-12              SCK         J2-12
PCS0       J2-6               PCS1        J2-6
GND        J2-14              GND         J2-14
Prepare the Demo
  1. Connect a Type-C USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal on PC for MCU-Link serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-IMX937
Hardware requirements
  • Micro USB cable

  • two FRDM-IMX937 boards

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

Connection as below:

MASTER(LPSPI7)                connect to        SLAVE(LPSPI7)
Pin Name    Board Location                      Pin Name    Board Location
PCS0        J18 pin 7                           PCS0        J18 pin 7
SCK         J18 pin 26                          SCK         J18 pin 26
SOUT        J18 pin 31                          SIN         J18 pin 9
SIN         J18 pin 9                           SOUT        J18 pin 31
GND         J18 pin 6                           GND         J18 pin 6

IMPORTANT: SOUT/SIN (MOSI/MISO) lines MUST be crossed as shown above.

Note: J18 is the 40-PIN GPIO HDR expansion connector. - J18-Pin7: LPSPI7_PCS0 (GPIO_IO04) - Chip Select - J18-Pin26: LPSPI7_SCK (GPIO_IO07) - Clock - J18-Pin31: LPSPI7_SOUT (GPIO_IO06) - MOSI (connects to slave SIN) - J18-Pin9: LPSPI7_SIN (GPIO_IO05) - MISO (connects to slave SOUT) - J18-Pin6: Common Ground (any GND pin on J18 can be used) - Each board must be powered independently - No IO expander configuration required for this example

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either cold boot your board or launch the debugger in your IDE to begin running the example.