flash_component_nor_spifi#
Overview#
nor flash demo shows the use of nor flash component to erase, program, and read an external nor flash device.
Supported Boards#
FRDM-MCXW23
Hardware requirements
Type-C USB cable
FRDM-MCXW23 Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the eeprom example in the terminal window:
SPIFI flash polling example started
All data written is correct!
SPIFI Polling example Finished!