mpi_loader_dsp_hello_world_loader#
Overview#
The mpi_loader_dsp_hello_world example demonstrates how to add secondary bootloader in CM33 application to load the multicore packed image, created by elftosb tool. Once the DSP image is loaded, CM33 can kick off it and both cores then execute in parallel.
Supported Boards#
EVK-MIMXRT595
Overview
The mpi_loader_dsp_hello_world example demonstrates how to add secondary bootloader in CM33 application to load the multicore packed image, created by elftosb tool. Once the DSP image is loaded, CM33 can kick off it and both cores then execute in parallel. The elftosb and blhost tool can be downloaded from nxp.com.
Hardware requirements
Micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board
DSP example boards\evkmimxrt595\dsp_examples\hello_world_usart\dsp should be built and we can then get dsp_reset_release.bin, dsp_text_release.bin and dsp_data_release.bin.
Build this example, and we can get sdk20-app.bin.
Copy all those binaries to elf2sb workspace “input_images” folder identified in mpi_loader_
.json. Copy mpi_loader_
.json to elf2sb workspace “image_config” folder. Execute elf2sb.exe with mpi_loader_
.json as parameter. E.g., (only 1 command needed depending on your build) elftosb.exe -V -d -f rt5xx -J workspace/image_config/mpi_loader_ram.json (for debug/release built sdk20-app.bin)
elftosb.exe -V -d -f rt5xx -J workspace/image_config/mpi_loader_flash.json (for flash_debug/flash_release built sdk20-app.bin)
In elf2sb workspace “output_images” folder, you can get the multicore packed image mpi_loader_dsp_hello_world.bin.
Write flash config block to flash offset 0x400 (address 0x08000400) and write mpi_loader_dsp_hello_world.bin to flash offset 0x1000 (address 0x08001000). E.g. with blhost tool, set board boot mode DIP to Serial ISP [1-ON, 2-OFF, 3-OFF], reset the board and use command window to communicate with it (need to identify the COM port).
blhost.exe -p COM20 – fill-memory 0x1c000 4 0xc0403004
blhost.exe -p COM20 – configure-memory 9 0x1c000
blhost.exe -p COM20 -t 100000 – flash-erase-region 0x08000000 0x100000
blhost.exe -p COM20 – fill-memory 0x1d000 4 0xf000000f
blhost.exe -p COM20 – configure-memory 0x9 0x1d000
blhost.exe -p COM20 – write-memory 0x08001000 workspace\output_images\mpi_loader_dsp_hello_world.bin
Set board boot mode to flash boot [1-OFF, 2-OFF, 3-ON]
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Reset the board and you will see the result.
Running the demo CM33
When the demo runs successfully, the terminal will display the following:
Hello World running on core 'Cortex-M33'
Hello World running on DSP core 'fusion_nxp1_s7_v11_prod'
EVK-MIMXRT685
Overview
The mpi_loader_dsp_hello_world example demonstrates how to add secondary bootloader in CM33 application to load the multicore packed image, created by elftosb tool. Once the DSP image is loaded, CM33 can kick off it and both cores then execute in parallel.
Hardware requirements
Micro USB cable
EVK-MIMXRT685 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
DSP example boards\evkmimxrt685\dsp_examples\hello_world_usart\hifi4 should be built and we can then get dsp_text_release.bin and dsp_data_release.bin.
Build this example, and we can get sdk20-app.bin.
Copy all those binaries to elf2sb workspace “input_images” folder identified in mpi_loader_
.json. Copy mpi_loader_
.json to elf2sb workspace “image_config” folder. Execute elf2sb.exe with mpi_loader_
.json as parameter. E.g., (only 1 command needed depending on your build) elftosb.exe -V -d -f rt6xx -J workspace/image_config/mpi_loader_ram.json (for debug/release built sdk20-app.bin)
elftosb.exe -V -d -f rt6xx -J workspace/image_config/mpi_loader_flash.json (for flash_debug/flash_release built sdk20-app.bin)
In elf2sb workspace “output_images” folder, you can get the multicore packed image mpi_loader_dsp_hello_world.bin.
Write flash config block to flash offset 0x400 (address 0x08000400) and write mpi_loader_dsp_hello_world.bin to flash offset 0x1000 (address 0x08001000). E.g. with blhost tool, set board boot mode DIP to Serial ISP [high, high, low], reset the board and use command window to communicate with it (need to identify the COM port).
blhost.exe -p COM29 – fill-memory 0x1c000 4 0xc1500051
blhost.exe -p COM29 – fill-memory 0x1c004 4 0x20000008
blhost.exe -p COM29 – configure-memory 9 0x1c000
blhost.exe -p COM29 -t 100000 – flash-erase-region 0x08000000 0x100000
blhost.exe -p COM29 – fill-memory 0x1d000 4 0xf000000f
blhost.exe -p COM29 – configure-memory 0x9 0x1d000
blhost.exe -p COM29 – write-memory 0x08001000 workspace\output_images\mpi_loader_dsp_hello_world.bin
Set board boot mode to flash portb boot [low, high, low]
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Reset the board and you will see the result.
Running the demo CM33
When the demo runs successfully, the terminal will display the following:
Hello World running on core 'Cortex-M33'
Hello World running on DSP core 'nxp_rt600_RI2020_5_newlib'
MIMXRT685-AUD-EVK
Overview
The mpi_loader_dsp_hello_world example demonstrates how to add secondary bootloader in CM33 application to load the multicore packed image, created by elftosb tool. Once the DSP image is loaded, CM33 can kick off it and both cores then execute in parallel.
Hardware requirements
Micro USB cable
MIMXRT685-AUD-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
DSP example boards\mimxrt685audevk\dsp_examples\hello_world_usart\hifi4 should be built and we can then get dsp_text_release.bin and dsp_data_release.bin.
Build this example, and we can get sdk20-app.bin.
Copy all those binaries to elf2sb workspace “input_images” folder identified in mpi_loader_
.json. Copy mpi_loader_
.json to elf2sb workspace “image_config” folder. Execute elf2sb.exe with mpi_loader_
.json as parameter. E.g., (only 1 command needed depending on your build) elftosb.exe -V -d -f rt6xx -J workspace/image_config/mpi_loader_ram.json (for debug/release built sdk20-app.bin)
elftosb.exe -V -d -f rt6xx -J workspace/image_config/mpi_loader_flash.json (for flash_debug/flash_release built sdk20-app.bin)
In elf2sb workspace “output_images” folder, you can get the multicore packed image mpi_loader_dsp_hello_world.bin.
Write flash config block to flash offset 0x400 (address 0x08000400) and write mpi_loader_dsp_hello_world.bin to flash offset 0x1000 (address 0x08001000). E.g. with blhost tool, set board boot mode DIP to Serial ISP [high, high, low](SW5 1-ON, 2-OFF, 3-OFF), reset the board and use command window to communicate with it (need to identify the COM port).
blhost.exe -p COM29 – fill-memory 0x1c000 4 0xc1000001
blhost.exe -p COM29 – fill-memory 0x1c004 4 0x20000006
blhost.exe -p COM29 – configure-memory 9 0x1c000
blhost.exe -p COM29 -t 100000 – flash-erase-region 0x08000000 0x100000
blhost.exe -p COM29 – fill-memory 0x1d000 4 0xf000000f
blhost.exe -p COM29 – configure-memory 0x9 0x1d000
blhost.exe -p COM29 – write-memory 0x08001000 workspace\output_images\mpi_loader_dsp_hello_world.bin
Set board boot mode to flash portb boot [low, high, low](SW5 1-ON, 2-OFF, 3-ON).
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Reset the board and you will see the result.
Running the demo CM33
When the demo runs successfully, the terminal will display the following:
Hello World running on core 'Cortex-M33'
Hello World running on DSP core 'nxp_rt600_RI2020_5_newlib'