adc12_low_power#
Overview#
The ADC Low Power Demo project is a demonstration program that uses the KSDK software. The microcontroller is set to a very low power stop (VLPS) mode, and every 500 ms an interrupt wakes up the ADC module and takes the current temperature sensor value of the microcontroller. While the temperature remains within boundaries, both LEDs are on. If the temperature is higher or lower than average, a led comes off. This demo provides an example to show how ADC works during a VLPS mode and a simple debugging.
Supported Boards#
FRDM-KE15Z
Hardware requirements
Micro USB cable
FRDM-KE15Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
ADC LOW POWER DEMO
The Low Power ADC project is designed to work with the Kinetis SDK.
1. Set your target board in a place where the temperature is constant.
2. Wait until two Led light turns on.
3. Increment or decrement the temperature to see the changes.
Wait two led on...
Enter any character to begin...
---> OK! Main process is running...!
Note:
when the temperature is raised: LED RED on, LED GREEN off.
when the temperature is reduced: LED GREEN on, LED RED off.
FRDM-KE16Z
Hardware requirements
Micro USB cable
FRDM-KE16Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
ADC LOW POWER DEMO
The Low Power ADC project is designed to work with the Kinetis SDK.
1. Set your target board in a place where the temperature is constant.
2. Wait until two Led light turns on.
3. Increment or decrement the temperature to see the changes.
Wait two led on...
Enter any character to begin...
---> OK! Main process is running...!
Note:
when the temperature is raised: LED RED on, LED GREEN off.
when the temperature is reduced: LED GREEN on, LED RED off.
FRDM-KE17Z
Hardware requirements
Micro USB cable
FRDM-KE17Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
ADC LOW POWER DEMO
The Low Power ADC project is designed to work with the Kinetis SDK.
1. Set your target board in a place where the temperature is constant.
2. Wait until two Led light turns on.
3. Increment or decrement the temperature to see the changes.
Wait two led on...
Enter any character to begin...
---> OK! Main process is running...!
Note:
when the temperature is raised: LED RED on, LED GREEN off.
when the temperature is reduced: LED GREEN on, LED RED off.
FRDM-KE17Z512
Hardware requirements
Micro USB cable
FRDM-KE17Z512 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-LINK terminal like:
ADC LOW POWER DEMO
The Low Power ADC project is designed to work with the Kinetis SDK.
1. Set your target board in a place where the temperature is constant.
2. Wait until two Led light turns on.
3. Increment or decrement the temperature to see the changes.
Wait two led on...
Enter any character to begin...
---> OK! Main process is running...!
Note:
when the temperature is raised: LED RED on, LED GREEN off.
when the temperature is reduced: LED GREEN on, LED RED off.