adc16_potentiometer#
Overview#
The ADC potentiometer demo application demonstrates how to read the analog value from a hardware potentiometer via the ADC peripheral.
Supported Boards#
TWR-KM34Z50MV3
Hardware requirements
Mini USB cable
TWR-KM34Z50MV3 board
Personal Computer
Board settings
Connect J21 1-2 to use potentiometer
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Roll the potentiometer to change the ADC value. When the example runs successfully, the following message is displayed in the terminal:
ADC16_DoAutoCalibration() Done.
The ADC16 output value is 1338.
The ADC16 output value is 1336.
The ADC16 output value is 1337.
.............................
.............................
TWR-KM34Z75M
Hardware requirements
Mini/micro USB cable
TWR-KM34Z75M board
Personal Computer
Board settings
Connect J21 1-2 to use potentiometer
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Roll the potentiometer to change the ADC value. When the example runs successfully, the following message is displayed in the terminal:
ADC16_DoAutoCalibration() Done.
The ADC16 output value is 216.
The ADC16 output value is 215.
The ADC16 output value is 215.
.............................
.............................
TWR-KM35Z75M
Hardware requirements
Micro USB cable
TWR-KM35Z75M board
Personal Computer
Board settings
Connect J21 1-2 to use potentiometer
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Roll the potentiometer to change the ADC value. When the example runs successfully, the following message is displayed in the terminal:
ADC16_DoAutoCalibration() Done.
The ADC16 output value is 216.
The ADC16 output value is 215.
The ADC16 output value is 215.
.............................
.............................