afe_qtimer
Overview
The AFE Example project is a demonstration program that uses the KSDK software. In this case the example provide two functions. Measure the voltage difference two pin of the channel 2 and 3. And monitor AC frequency on two pins of channel 2.