xbar_aoi_peripheral#
Overview#
The XBAR AOI Peripheral demo application demonstrates the usage of the XBAR, AOI peripheral to combine interrupt from CMP and PIT. If the button is pressed(CMP interrupt) and the PIT periodic interrupt occurs a message is printed.
Supported Boards#
EVKB-IMXRT1050
Hardware requirements
Mini/micro USB cable
IMXRT1050-EVKB board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the xbar aoi demo in the terminal window:
XBAR and AOI Peripheral Demo: Start...
Then change CMP analog input.
- CMP1_IN0 (J23-5) connected to VCC =3.3V (J24-8): XBAR interrupt occurred
- CMP1_IN0 (J23-5) connected to GND (J24-7)): XBAR interrupt stopped
XBAR interrupt occurred
XBAR interrupt occurred
MIMXRT1060-EVKB
Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKB board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the xbar aoi demo in the terminal window:
XBAR and AOI Peripheral Demo: Start...
Then change CMP analog input.
- CMP1_IN0 (J33-5) connected to VCC =3.3V (J17-8): XBAR interrupt occurred
- CMP1_IN0 (J33-5) connected to GND (J17-7)): XBAR interrupt stopped
XBAR interrupt occurred
XBAR interrupt occurred
MIMXRT1060-EVKC
Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKC board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the xbar aoi demo in the terminal window:
XBAR and AOI Peripheral Demo: Start...
Then change CMP analog input.
- CMP1_IN0 (J33-5) connected to VCC =3.3V (J17-8): XBAR interrupt occurred
- CMP1_IN0 (J33-5) connected to GND (J17-7)): XBAR interrupt stopped
XBAR interrupt occurred
XBAR interrupt occurred
EVK-MIMXRT1020
Hardware requirements
Mini/micro USB cable
MIMXRT1020-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the xbar aoi demo in the terminal window:
XBAR and AOI Peripheral Demo: Start...
Then change CMP analog input.
- CMP1_IN0 (J17-7) connected to VCC =3.3V (J19-8): XBAR interrupt occurred
- CMP1_IN0 (J17-7) connected to GND (J19-7): XBAR interrupt stopped
XBAR interrupt occurred
XBAR interrupt occurred
MIMXRT1024-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1024-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the xbar aoi demo in the terminal window:
XBAR and AOI Peripheral Demo: Start...
Then change CMP analog input.
- CMP1_IN0 (J17-14) connected to VCC =3.3V (J19-16): XBAR interrupt occurred
- CMP1_IN0 (J17-14) connected to GND (J19-14): XBAR interrupt stopped
XBAR interrupt occurred
XBAR interrupt occurred
MIMXRT1040-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1040-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the xbar aoi demo in the terminal window:
XBAR and AOI Peripheral Demo: Start...
Then change CMP analog input.
- CMP1_IN0 (J17-9) connected to VCC =3.3V (J32-4): XBAR interrupt occurred
- CMP1_IN0 (J17-9) connected to GND (J32-6)): XBAR interrupt stopped
XBAR interrupt occurred
XBAR interrupt occurred
EVK-MIMXRT1064
Hardware requirements
Mini/micro USB cable
MIMXRT1064-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the xbar aoi demo in the terminal window:
XBAR and AOI Peripheral Demo: Start...
Then change CMP analog input.
- CMP1_IN0 (J23-5) connected to VCC =3.3V (J24-8): XBAR interrupt occurred
- CMP1_IN0 (J23-5) connected to GND (J24-7)): XBAR interrupt stopped
XBAR interrupt occurred
XBAR interrupt occurred