biss#
Overview#
This example demonstrates how to access BiSS device.
Supported Boards#
IMX943-EVK
Hardware requirements
USB Type-C cable
i.MX943-EVK board
Personal Computer
Power supply 24V
Motor control board (FRDM-LVPMSM-FA)
BiSS sensor
Board settings
Insert FRDM-LVPMSM-FA board into Arduino interface of motor control 2. Connect BiSS sensor and power supply to FRDM-LVPMSM-FA
BiSS point-to-point connection:
INSTANCE(FRDM-LVPMSM-FA) CONNECTS TO INSTANCE(BiSS sensor)
Pin Name Board Location Signal Name
ENC_CLK_P J70-2 MASTER_CLOCK_INPUT_P
ENC_CLK_N J70-7 MASTER_CLOCK_INPUT_N
ENC_DATA_IN_P J70-3 SLAVE_DATA_P
ENC_DATA_IN_N J70-8 SLAVE_DATA_N
VENC J70-1 VDC - Power supply voltage
GND J70-6 GND
BiSS daisy-chain connection:
INSTANCE(FRDM-LVPMSM-FA) CONNECTS TO INSTANCE(BiSS sensor)
Pin Name Board Location Signal Name
ENC_CLK_P J70-2 MASTER_CLOCK_INPUT_P
ENC_CLK_N J70-7 MASTER_CLOCK_INPUT_N
ENC_DATA_IN_P J70-3 SLAVE_DATA_P
ENC_DATA_IN_N J70-8 SLAVE_DATA_N
ENC_DATA_IO_P J70-4 SLAVE_DATA_INPUT_P
ENC_DATA_IO_N J70-9 SLAVE_DATA_INPUT_N
VENC J70-1 VDC - Power supply voltage
GND J70-6 GND
SW90 setting:
SW[1-2] ON:OFF Full duplex
SW[3] OFF Echo Enabled
SW[4] ON ENDAT is used.
SW30 setting - Select the appropriate voltage based on the properties of the sensor
SW[1] ON 3.3V
SW[2] ON 5.2V
SW[3] ON 9V
SW[4] ON 12V
Jumpers:
J300: pin1 <--> pin2
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
BiSS test example.
This example use one board as BiSS master and connect to the BiSS encoder.
Please make sure you make the correct line connection. Basically, the connection is:
MA -- BISS Clock Line Output
MO -- BISS Data Line Output
SL -- BISS Data Line Input
Select the encoder command from following:
1: Dump slave position
2: Dump registers
3: Enable instruction trigger
4: Enable AGS repetition trigger
5: Enable timeout trigger
6: GETSENS pin trigger
7: Reset BiSS-C
8: Re-scan BiSS bus
9: Dump slave information
0: Test Performance
Input command values: