MCUXpresso SDK Documentation

Hiperface DSL

Hiperface DSL#

Overview#

This example demonstrates how to access Hiperface DSL device.

Supported Boards#

IMX943-EVK
Hardware requirements
  • USB Type-C cable

  • i.MX943-EVK board

  • Personal Computer

  • Power supply 24V

  • Motor control board (FRDM-LVPMSM-FA)

  • Hiperface sensor

Board settings

Insert FRDM-LVPMSM-FA board into Arduino interface of motor control 2. Connect EnDat3 sensor and power supply to FRDM-LVPMSM-FA

EnDat3 connection:

Pin Name        Board Location              Signal Name
ENC_DATA_IO_VENC_P      J70-5                     DATA_P
ENC_DATA_IO_CENC_N      J70-10                    DATA_N

SW90 setting:

SW[1-2] OFF:ON Half duplex
SW[3]   OFF    Echo Enabled
SW[4]   ON     ENDAT is used.

SW30 setting - Select the appropriate voltage based on the properties of the sensor

SW[1] ON 3.3V
SW[2] ON 5.2V
SW[3] ON 9V
SW[4] ON 12V

The Jumper settings:

To make the example work, the below jumpers should be connected:
Jumper setting:
    J72:   pin3 <--> pin 1
    J72:   pin4 <--> pin 2
    J73:   pin2 <--> pin 1
    J300:  pin2 <--> pin 1
Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW1(SYS_PWR) to power on the board.

  2. Connect a micro USB cable between the host PC and the J15(FTDI_DEBUG) USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.