adc16_continuous_edma

Overview

The ADC16 continuous EDMA demo application demonstrates the usage of the ADC and EDMA peripheral while in a continuous mode. The ADC16 is first set to continuous mode. In continuous convert configuration, only the initial rising-edge to launch continuous conversions is observed, and until conversion is aborted, the ADC16 continues to do conversions on the same SCn register that initiated the conversion. EDMA request will be asserted during an ADC16 conversion complete event noted when any of the SC1n[COCO] flags is asserted. EDMA will transfer ADC16 results to memory and if users press any key, demo will average ADC16 results stored in memory and print average on the terminal.

Supported Boards