adc_etc_hardware_trigger_conv#
Overview#
The adc_etc_hardware_trigger_conv example shows how to use the ADC_ETC to generate a ADC trigger by PIT channel0 trigger.
Every 1 second, PIT channel0 would send a trigger signal to ADC_ETC, which can arbitrate and manage multiple external triggers, and ADC_ETC would generate ADC trigger.
In this example, the ADC is configured with hardware trigger. Once ADC gets the trigger from the ADC_ETC, the conversion goes, then the ADC_ETC ISR would be executed.
Supported Boards#
EVKB-IMXRT1050
Hardware requirements
Mini/micro USB cable
EVKB-IMXRT1050 board
Personal Computer
Board settings
ADC0_IN15 and ADC0_IN0 are ADC inputs. Please sample voltage by J23-1 and J23-2 pins.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC_ETC_Hardware_Trigger_Conv Example Start!
ADC_DoAutoCalibration() Done.
ADC Full Range: XXXX
Please press any key to get user channel's ADC value.
ADC conversion value is 107 and 3882
ADC conversion value is 103 and 3884
ADC conversion value is 104 and 3880
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 104 and 3882
ADC conversion value is 104 and 3882
...
MIMXRT1060-EVKB
Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKB board
Personal Computer
Board settings
ADC0_IN15 and ADC0_IN0 are ADC inputs. Please sample voltage by J33-1 and J33-2 pins.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC_ETC_Hardware_Trigger_Conv Example Start!
ADC_DoAutoCalibration() Done.
ADC Full Range: XXXX
Please press any key to get user channel's ADC value.
ADC conversion value is 107 and 3882
ADC conversion value is 103 and 3884
ADC conversion value is 104 and 3880
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 104 and 3882
ADC conversion value is 104 and 3882
...
MIMXRT1060-EVKC
Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKC board
Personal Computer
Board settings
ADC0_IN15 and ADC0_IN0 are ADC inputs. Please sample voltage by J33-1 and J33-2 pins.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC_ETC_Hardware_Trigger_Conv Example Start!
ADC_DoAutoCalibration() Done.
ADC Full Range: XXXX
Please press any key to get user channel's ADC value.
ADC conversion value is 107 and 3882
ADC conversion value is 103 and 3884
ADC conversion value is 104 and 3880
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 104 and 3882
ADC conversion value is 104 and 3882
...
EVK-MIMXRT1010
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1010 board
Personal Computer
Board settings
ADC1_IN07 and ADC1_IN14 are ADC inputs. Please sample voltage by J26-2 and J26-8 pins.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC_ETC_Hardware_Trigger_Conv Example Start!
ADC_DoAutoCalibration() Done.
ADC Full Range: XXXX
Please press any key to get user channel's ADC value.
ADC conversion value is 107 and 3882
ADC conversion value is 103 and 3884
ADC conversion value is 104 and 3880
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 104 and 3882
ADC conversion value is 104 and 3882
...
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
EVK-MIMXRT1015
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1015 board
Personal Computer
Board settings
ADC1_IN10 and ADC1_IN13 are ADC inputs. Please sample voltage by J18-1 and J18-4 pins.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC_ETC_Hardware_Trigger_Conv Example Start!
ADC_DoAutoCalibration() Done.
ADC Full Range: XXXX
Please press any key to get user channel's ADC value.
ADC conversion value is 107 and 3882
ADC conversion value is 103 and 3884
ADC conversion value is 104 and 3880
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 104 and 3882
ADC conversion value is 104 and 3882
...
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
EVK-MIMXRT1020
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1020 board
Personal Computer
Board settings
ADC1_IN10 and ADC1_IN11 are ADC inputs. Please sample voltage by J18-1 and J18-2 pins.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC_ETC_Hardware_Trigger_Conv Example Start!
ADC_DoAutoCalibration() Done.
ADC Full Range: XXXX
Please press any key to get user channel's ADC value.
ADC conversion value is 107 and 3882
ADC conversion value is 103 and 3884
ADC conversion value is 104 and 3880
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 104 and 3882
ADC conversion value is 104 and 3882
...
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
MIMXRT1024-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1024-EVK board
Personal Computer
Board settings
ADC1_IN10 and ADC1_IN11 are ADC inputs. Please sample voltage by J18-2 and J18-4 pins.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC_ETC_Hardware_Trigger_Conv Example Start!
ADC_DoAutoCalibration() Done.
ADC Full Range: XXXX
Please press any key to get user channel's ADC value.
ADC conversion value is 107 and 3882
ADC conversion value is 103 and 3884
ADC conversion value is 104 and 3880
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 104 and 3882
ADC conversion value is 104 and 3882
...
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
MIMXRT1040-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1040-EVK board
Personal Computer
Board settings
ADC1_IN9 and ADC1_IN10 are ADC inputs. Please sample voltage by J33-3 and J33-4 pins.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC_ETC_Hardware_Trigger_Conv Example Start!
ADC_DoAutoCalibration() Done.
ADC Full Range: XXXX
Please press any key to get user channel's ADC value.
ADC conversion value is 107 and 3882
ADC conversion value is 103 and 3884
ADC conversion value is 104 and 3880
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 104 and 3882
ADC conversion value is 104 and 3882
...
EVK-MIMXRT1064
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1064 board
Personal Computer
Board settings
ADC0_IN15 and ADC0_IN0 are ADC inputs. Please sample voltage by J23-1 and J23-2 pins.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC_ETC_Hardware_Trigger_Conv Example Start!
ADC_DoAutoCalibration() Done.
Please press any key to get user channel's ADC value.
ADC conversion value is 107 and 3882
ADC conversion value is 103 and 3884
ADC conversion value is 104 and 3880
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 88 and 3890
ADC conversion value is 104 and 3882
ADC conversion value is 104 and 3882
...