AUDMIX with SAI Codec Example#
Overview#
This example demonstrates how to use the AUDMIX (Audio Mixer) peripheral with SAI interfaces to mix audio streams. The AUDMIX peripheral is designed to mix two audio streams, each with up to 8 audio channels, producing a mixed output audio stream.
Description#
The example initializes three SAI peripherals:
SAI1: Configured as TDM1 input to AUDMIX
SAI2: Configured as TDM2 input to AUDMIX
After initialization, the example checks if the TDM streams from SAI1 and SAI2 are synchronized (both clock frequency and frame rate). If synchronized, it enables mixed output mode and demonstrates attenuation control. If not synchronized, it falls back to using only TDM1 as the output source.
The example demonstrates:
Initialization and configuration of the AUDMIX peripheral
Checking synchronization between TDM streams
Configuring mixed output when streams are synchronized
Applying and controlling attenuation profiles
Falling back to single stream output when synchronization fails
Hardware Requirements#
An NXP development board with AUDMIX and SAI peripherals
Audio codec connected to the SAI interfaces
Audio output device (headphones or speakers)
Software Requirements#
MCUXpresso SDK
Development environment (MCUXpresso IDE, IAR, Keil, etc.)
Setup#
Connect the development board to your computer
Build and flash the example to your board
Connect an audio output device to hear the mixed audio
Running the Example#
After flashing the example, open a terminal to view debug messages
The example will initialize the SAI and AUDMIX peripherals
It will check if TDM streams are synchronized and report the status
If synchronized, it will enable mixed output and demonstrate attenuation
If not synchronized, it will use only TDM1 as the output source
The example will report completion when finished
Expected Output#
AUDMIX example started!
TDM clock match status: Matched
TDM frame rate match status: Matched
TDM streams are synchronized, enabling mixed output.
AUDMIX example completed!
Or if streams are not synchronized:
AUDMIX example started!
TDM clock match status: Mismatched
TDM frame rate match status: Mismatched
TDM streams are not synchronized, using TDM1 output only.
AUDMIX example completed!
Troubleshooting#
If TDM streams are not synchronized, check the SAI configuration to ensure both SAI1 and SAI2 are configured with the same sample rate, bit width, and channel count.
If no audio is heard, verify the audio codec connections and configuration.
Check the debug console output for status information.
Customization#
You can modify the example to:
Change the audio sample rate by adjusting the
sampleRate_HzparameterModify the attenuation profile by changing the attenuation configuration parameters
Experiment with different output width settings (16/18/20/24-bit)
Try different attenuation directions and timing
Limitations#
The example assumes that audio data is being provided to the SAI interfaces
Both TDM streams must have the same audio sample rate and number of channels for mixing to work properly
Supported Boards#
IMX952-EVK
Hardware requirements
Micro USB cable
IMX952-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Headphone
Board settings
No special settings are required.
Prepare the Demo
Note: single boot with Linux BSP is required. SAI3, SAI6 and EDMA4 are modules of WAKEUPMIX, A core and Linux BSP is responsible to configure proper permissions with TRDC.
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example
Running the demo
When the demo runs successfully, you can hear the tone and the log would be seen on the terminal like:
AUDMIX example started!
TDM streams are synchronized, enabling mixed output.
AUDMIX example completed!