MCUXpresso SDK Documentation

acmp_interrupt

acmp_interrupt#

Overview#

In hw_trig example, a counter is used to generate a 10KHz, 70% duty cycle PWM, and a trigger is generated at 50% of the PWM period. This trigger is routed to bctu as the hardware trigger source, which is then trigger ADC to convert.

Supported Boards#