MCUXpresso SDK Documentation

capt_acomp

capt_acomp#

Overview#

This example shows how to capture touch data using CAPT poll-now mode. Comparing with the capt_basic example, this example uses ACOMP instead of GPIO in measurement stage. In this mode, application trigger the polling round, after polling round, the CAPT stops and notifies application by interrupt or register status. In this example, application poll the enabled pins one by one, after all pins are sampled, the result are shown in the debug terminal. Then application starts to sample all the enabled pins again.

When the example runs, the sampled data is shown in the terminal. When electrode plate is touched, the sampled data changes too.

Supported Boards#

LPC845BREAKOUT
Hardware requirements
  • Micro USB cable

  • LPC845 Breakout board

  • Personal Computer

Board settings

Make sure R23 is on the LPC845 Breakout board.

Prepare the demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board.

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The CAPT sample data is shown in the terminal, touch the electrode plate to see sample data change.

LPCXpresso804
Toolchain supported
  • IAR embedded Workbench 8.22.1

  • Keil MDK 5.24a

  • MCUXpresso10.2.0

Hardware requirements
  • Micro USB cable

  • LPCXpresso804 board

  • CapTouch Shield board

  • Personal Computer

Board settings

Remove JP3, JP21, JP22, JP23, JP25 and C13 on LPCXpresso804 board. Short R6 on CapTouch Shield board

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the CMSIS DAP USB port (CN2) on the target board.

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The CAPT sample data is shown in the terminal, touch the electrode plate to see sample data change.