csi_raw8#
Overview#
This project shows how to receive the camera RAW8 data using CSI driver. In this example, the RAW8 data is convert to RGB565 data, then shown in the panel.
Supported Boards#
EVKB-IMXRT1050
Hardware requirements
Mini/micro USB cable
EVKB-IMXRT1050 board
Personal Computer
RK043FN02H-CT or RK043FN66HS-CT6 LCD board (RK043FN02H-CT and RK043FN66HS-CT6 are compatible)
MT9M114 module
Board settings
Connect the RK043FN02H-CT or RK043FN66HS-CT6 to board.
Connect the MT9M114 camera module.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Note: This project only support MT9M114.
Running the demo
When the demo runs successfully, the camera received pictures are shown in the LCD.
MIMXRT1060-EVKB
Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKB board
Personal Computer
RK043FN02H-CT or RK043FN66HS-CT6 LCD board (RK043FN02H-CT and RK043FN66HS-CT6 are compatible)
MT9M114 module
Board settings
Connect the RK043FN02H-CT or RK043FN66HS-CT6 to board.
Connect the MT9M114 camera module.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Note: This project only support MT9M114.
Running the demo
When the demo runs successfully, the camera received pictures are shown in the LCD.
MIMXRT1060-EVKC
Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKC board
Personal Computer
RK043FN02H-CT or RK043FN66HS-CT6 LCD board (RK043FN02H-CT and RK043FN66HS-CT6 are compatible)
MT9M114 module
Board settings
Connect the RK043FN02H-CT or RK043FN66HS-CT6 to board.
Connect the MT9M114 camera module.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Note: This project only support MT9M114.
Running the demo
When the demo runs successfully, the camera received pictures are shown in the LCD.
EVK-MIMXRT1064
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1064 board
Personal Computer
RK043FN02H-CT or RK043FN66HS-CT6 LCD board (RK043FN02H-CT and RK043FN66HS-CT6 are compatible)
MT9M114 module
Board settings
Connect the RK043FN02H-CT or RK043FN66HS-CT6 to board.
Connect the MT9M114 camera module.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Note: This project only support MT9M114.
Running the demo
When the demo runs successfully, the camera received pictures are shown in the LCD.