edma_wrap_address

Overview

The EDMA wrap address example is a simple demonstration program that uses the SDK software. It excuates wrap transfer from source buffer to destination buffer using the SDK EDMA drivers. The purpose of this example is to show how to use the EDMA modulo feature and to provide a simple example for debugging and further development.

Supported Boards