MCUXpresso SDK Documentation

dsc_i2c_interrupt_b2b_transfer_slave

dsc_i2c_interrupt_b2b_transfer_slave#

Overview#

The i2c_interrupt_b2b_transfer_slave example shows how to use i2c driver as slave to do board to board transfer with interrupt:

In this example, one i2c instance as slave and another i2c instance on the other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.

Supported Boards#