pit_basic_generic#
Overview#
The pit_basic_generic project is a simple demonstration program of the SDK PIT driver
(drivers/dsc_pit) using a platform-neutral ISR convention. It sets up the PIT
hardware block to trigger a periodic interrupt every 1 second. When the PIT interrupt
is triggered, a message is printed on the UART terminal and an LED is toggled on the
board.
This example uses the same drivers/dsc_pit source as the pit_basic example,
but provides a platform-neutral main file with a standard C ISR and no DSC-specific
interrupt conventions (no #pragma interrupt, no __CWCC__, no DSC_INTERRUPT_*
variants, no INTC_SetFastIRQVectorHandler), so customers on any platform that
reuses this driver see code that is directly relevant to their target.