MCUXpresso SDK Documentation

qtmr_outputpwm

qtmr_outputpwm#

Overview#

The QTMR project is a demonstration program of the SDK QTMR driver’s output variable frequency pwm feature by interrupt. The example also up one QTMR channel to output pwm. The user should probe a 50Khz PWM signal output with 50% dutycycle with a oscilloscope. The user can enter a value to update the Duty cycle.

Supported Boards#