MCUXpresso SDK Documentation

dspi_interrupt_b2b_slave

dspi_interrupt_b2b_slave#

Overview#

The dspi_interrupt_b2b example shows how to use DSPI driver in interrupt way:

In this example , we need two boards , one board used as DSPI master and another board used as DSPI slave. The file ‘dspi_interrupt_b2b_slave.c’ includes the DSPI slave code. This example does not use the transactional API in DSPI driver. It’s a demonstration that how to use the interrupt in KSDK driver.

  1. DSPI master send/received data to/from DSPI slave in interrupt . (DSPI Slave using interrupt to receive/send the data)

Supported Boards#