MCUXpresso SDK Documentation

ecspi_polling_b2b_transfer_master

ecspi_polling_b2b_transfer_master#

Overview#

The ecspi_polling_b2b_transfer example shows how to use ECSPI driver in polling way:

In this example , we need two boards, one board used as ECSPI master and another board used as ECSPI slave. The file ‘ecspi_polling_b2b_transfer_master.c’ includes the ECSPI master code.

  1. ECSPI master send/received data to/from ECSPI slave in polling . (ECSPI Slave using interrupt to receive/send the data)

Supported Boards#