MCUXpresso SDK Documentation

pflash_swap#

Overview#

The flash_swap example shows how to use flash swap feature:

Running the demo#

When the example runs successfully, you can see the similar information from the terminal as below.

PFLASH Swap example Start PFlash Information: Total Program Flash Size: xx KB, Hex: (xx) Total Program Flash Block Count: xx Program Flash Sector Size: xx KB, hex: (xx) Flash is xx Original swap indicator address: xx Current swap system status: xx Validating the backup example image… Backup example image is invalid Start to program backup example image Finish programming backup example image Checking the system status… It is first swap for the system Start to erase test data on lower pflash before swapping system Finish erasing test data Start to program backup test data on upper pflash Finish programming backup test data Start to swap the system

Perform a system reset

FLASH Swap example Start PFlash Information: Total Program Flash Size: xx KB, Hex: (xx) Total Program Flash Block Count: xx Program Flash Sector Size: xx KB, hex: (xx) Flash is xx Original swap indicator address: xx Current swap system status: xx Validating the backup example image… Backup example image is valid Checking the system status… The system has been swapped successfully Start to erase test data on lower pflash before exiting this example Finish erasing test data

End of PFLASH Swap example

Supported Boards#

FRDM-KE17Z512
Hardware requirements
  • Micro USB cable

  • FRDM-KE17Z512 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

These instructions are displayed/shown on the terminal window:

 PFLASH Swap example Start
 PFlash Information: 
 Total Program Flash Size: xx KB, Hex: (xx)
 Total Program Flash Block Count: xx
 Program Flash Sector Size: xx KB, hex: (xx)
 Flash is xx
 Original swap indicator address: xx
 Current swap system status: xx
 Validating the backup example image...
 Backup example image is invalid 
 Start to program backup example image
 Finish programming backup example image
 Checking the system status...
 It is first swap for the system
 Start to erase test data on lower pflash before swapping system
 Finish erasing test data
 Start to program backup test data on upper pflash
 Finish programming backup test data
 Start to swap the system

 Perform a system reset

 FLASH Swap example Start
 PFlash Information: 
 Total Program Flash Size: xx KB, Hex: (xx)
 Total Program Flash Block Count: xx
 Program Flash Sector Size: xx KB, hex: (xx)
 Flash is xx
 Original swap indicator address: xx
 Current swap system status: xx
 Validating the backup example image...
 Backup example image is valid
 Checking the system status...
 The system has been swapped successfully
 Start to erase test data on lower pflash before exiting this example
 Finish erasing test data

 End of PFLASH Swap example