MCUXpresso SDK Documentation

flexcan_efifo_interrupt_transfer_low_level

flexcan_efifo_interrupt_transfer_low_level#

Overview#

The flexcan_efifo_interrupt_transfer_low_level example shows how to use FlexCAN Enhanced Rx FIFO with low-level hardware APIs in none-blocking interrupt way:

This example demonstrates direct hardware access without using the FlexCAN transfer layer. It implements a custom ISR that calls hardware APIs directly to handle Enhanced Rx FIFO interrupts efficiently. The ISR uses a ring buffer design to manage received frames between interrupt context and main loop.

The example will config one FlexCAN Message Buffer to Tx Message Buffer and setup Enhanced Rx FIFO. After that, the example will send some CAN FD Messages(default 4 frames) from Tx Message Buffer to Enhanced Rx FIFO through internal loopback interconnect. The sent and received message will be print out to terminal

2 boards are required to be connected through CAN bus. Endpoint A(board A) send a CAN Message to Endpoint B(board B) when user press space key in terminal. Endpoint B receives the message by Enhanced Rx FIFO, and print the message content to terminal after receive CAN FD messages.

Supported Boards#

KW47-EVK
Hardware requirements
  • Type-C USB cable

  • KW47-EVK Board

  • Personal Computer

Board settings

Example requires 2 sets of boards, each of them is mounted with the base board. To make example work, connections needed to be as follows on each base board:

Board to board connections needed to be as follows:

        Node A           connect to      Node B
Pin Name   Board Location         Pin Name    Board Location
CANH       J10-1                  CANH        J10-1
CANL       J10-2                  CANL        J10-2
GND        J10-4                  GND         J10-4

Note: Plug the 12V power supply on J9 to supply the P5V_CAN.

Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

This message displays on the node A terminal:

FlexCAN Enhanced Rx FIFO low-level interrupt example.
Board to board mode.
Node B: Enhanced Rx FIFO used for Rx (frame count unknown in advance).
Node A: Message buffer 0 used for Tx.
Please select local node as A or B:
Note: Node B should start first.
Node:A
Please input the number of CAN FD messages to be send and end with enter.
8
Send Msg0 to Enhanced Rx FIFO: word0 = 0x0, word1 = 0x55, id = 0x123.
Send Msg1 to Enhanced Rx FIFO: word0 = 0x1, word1 = 0x55, id = 0x124.
Send Msg2 to Enhanced Rx FIFO: word0 = 0x2, word1 = 0x55, id = 0x125.
Send Msg3 to Enhanced Rx FIFO: word0 = 0x3, word1 = 0x55, id = 0x126.
Send Msg4 to Enhanced Rx FIFO: word0 = 0x4, word1 = 0x55, id = 0x123.
Send Msg5 to Enhanced Rx FIFO: word0 = 0x5, word1 = 0x55, id = 0x124.
Send Msg6 to Enhanced Rx FIFO: word0 = 0x6, word1 = 0x55, id = 0x125.
Send Msg7 to Enhanced Rx FIFO: word0 = 0x7, word1 = 0x55, id = 0x126.
Transmission done.

....

This message displays on the node B terminal:

FlexCAN Enhanced Rx FIFO low-level interrupt example.
Board to board mode.
Node B: Enhanced Rx FIFO used for Rx (frame count unknown in advance).
Node A: Message buffer 0 used for Tx.
Please select local node as A or B:
Note: Node B should start first.
Node:B
Waiting for frames from Node A...

Receive frame from Enhanced Rx FIFO: word0 = 0x0, word1 = 0x55, ID Filter Hit: 0, Time stamp: 1971.
Receive frame from Enhanced Rx FIFO: word0 = 0x1, word1 = 0x55, ID Filter Hit: 1, Time stamp: 11038.
Receive frame from Enhanced Rx FIFO: word0 = 0x2, word1 = 0x55, ID Filter Hit: 2, Time stamp: 20106.
Receive frame from Enhanced Rx FIFO: word0 = 0x3, word1 = 0x55, ID Filter Hit: 3, Time stamp: 29173.
Receive frame from Enhanced Rx FIFO: word0 = 0x4, word1 = 0x55, ID Filter Hit: 0, Time stamp: 38241.
Receive frame from Enhanced Rx FIFO: word0 = 0x5, word1 = 0x55, ID Filter Hit: 1, Time stamp: 47308.
Receive frame from Enhanced Rx FIFO: word0 = 0x6, word1 = 0x55, ID Filter Hit: 2, Time stamp: 56375.
Receive frame from Enhanced Rx FIFO: word0 = 0x7, word1 = 0x55, ID Filter Hit: 3, Time stamp: 65443.

....
FRDM-MCXE31B
Hardware requirements
  • Micro USB cable

  • FRDM-MCXE31B Board

  • Personal Computer

Board settings

The example requires 2 sets of boards, each of them is mounted with the base board. To make example work, connections needed to be as follows on each base board:

Board to board connections needed to be as follows:

        Node A           connect to      Node B
Pin Name   Board Location         Pin Name    Board Location
CANH       J17-1                  CANH        J17-1
CANL       J17-2                  CANL        J17-2
GND        J17-4                  GND         J17-4
Prepare the Demo
  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

This message displays on the node A terminal:

FlexCAN Enhanced Rx FIFO low-level interrupt example.
Board to board mode.
Node B: Enhanced Rx FIFO used for Rx (frame count unknown in advance).
Node A: Message buffer 0 used for Tx.
Please select local node as A or B:
Note: Node B should start first.
Node:A
Please input the number of CAN FD messages to be send and end with enter.
8
Send Msg0 to Enhanced Rx FIFO: word0 = 0x0, word1 = 0x55, id = 0x123.
Send Msg1 to Enhanced Rx FIFO: word0 = 0x1, word1 = 0x55, id = 0x124.
Send Msg2 to Enhanced Rx FIFO: word0 = 0x2, word1 = 0x55, id = 0x125.
Send Msg3 to Enhanced Rx FIFO: word0 = 0x3, word1 = 0x55, id = 0x126.
Send Msg4 to Enhanced Rx FIFO: word0 = 0x4, word1 = 0x55, id = 0x123.
Send Msg5 to Enhanced Rx FIFO: word0 = 0x5, word1 = 0x55, id = 0x124.
Send Msg6 to Enhanced Rx FIFO: word0 = 0x6, word1 = 0x55, id = 0x125.
Send Msg7 to Enhanced Rx FIFO: word0 = 0x7, word1 = 0x55, id = 0x126.
Transmission done.

....

This message displays on the node B terminal:

FlexCAN Enhanced Rx FIFO low-level interrupt example.
Board to board mode.
Node B: Enhanced Rx FIFO used for Rx (frame count unknown in advance).
Node A: Message buffer 0 used for Tx.
Please select local node as A or B:
Note: Node B should start first.
Node:B
Waiting for frames from Node A...

Receive frame from Enhanced Rx FIFO: word0 = 0x0, word1 = 0x55, ID Filter Hit: 0, Time stamp: 1971.
Receive frame from Enhanced Rx FIFO: word0 = 0x1, word1 = 0x55, ID Filter Hit: 1, Time stamp: 11038.
Receive frame from Enhanced Rx FIFO: word0 = 0x2, word1 = 0x55, ID Filter Hit: 2, Time stamp: 20106.
Receive frame from Enhanced Rx FIFO: word0 = 0x3, word1 = 0x55, ID Filter Hit: 3, Time stamp: 29173.
Receive frame from Enhanced Rx FIFO: word0 = 0x4, word1 = 0x55, ID Filter Hit: 0, Time stamp: 38241.
Receive frame from Enhanced Rx FIFO: word0 = 0x5, word1 = 0x55, ID Filter Hit: 1, Time stamp: 47308.
Receive frame from Enhanced Rx FIFO: word0 = 0x6, word1 = 0x55, ID Filter Hit: 2, Time stamp: 56375.
Receive frame from Enhanced Rx FIFO: word0 = 0x7, word1 = 0x55, ID Filter Hit: 3, Time stamp: 65443.

....