iuart_auto_baudrate_detect#
Overview#
The uart_auto_baudrate_detect example shows how to use uart auto baud rate detect feature:
In this example, one uart instance connect to PC through uart. First, we should send characters a or A to board. The boars will set baud rate automatic. After baud rate has set, the board will send back all characters that PC send to the board.
Supported Boards#
EVK-MIMX8MM
Hardware requirements
Micro USB cable
MIMX8MM6-EVK board
J-Link Debug Probe
12V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 12V power supply and J-Link Debug Probe to the board, switch SW101 to power on the board
Connect a USB cable between the host PC and the J901 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
Set any baud rate in your terminal, and send character a or A to board, then
When the demo runs successfully, the log would be seen on the debug terminal like:
UART has detect one character A
Baud rate has been set automatic!
Board will send back received characters
EVK-MIMX8MN
Hardware requirements
Micro USB cable
MIMX8MN6-EVK board
J-Link Debug Probe
12V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 12V power supply and J-Link Debug Probe to the board, switch SW101 to power on the board
Connect a USB cable between the host PC and the J901 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
Set any baud rate in your terminal, and send character a or A to board, then
When the demo runs successfully, the log would be seen on the debug terminal like:
UART has detect one character A
Baud rate has been set automatic!
Board will send back received characters
EVK-MIMX8MNDDR3L
Hardware requirements
Micro USB cable
MIMX8MN6-EVK board
J-Link Debug Probe
12V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 12V power supply and J-Link Debug Probe to the board, switch SW101 to power on the board
Connect a USB cable between the host PC and the J901 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
Set any baud rate in your terminal, and send character a or A to board, then
When the demo runs successfully, the log would be seen on the debug terminal like:
UART has detect one character A
Baud rate has been set automatic!
Board will send back received characters
EVK-MIMX8MP
Hardware requirements
Micro USB cable
EVK-MIMX8M Plus board
J-Link Debug Probe
12V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 12V power supply and J-Link Debug Probe to the board, switch SW3 to power on the board
Connect a USB cable between the host PC and the J23 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
Set any baud rate in your terminal, and send character a or A to board, then
When the demo runs successfully, the log would be seen on the debug terminal like:
UART has detect one character A
Baud rate has been set automatic!
Board will send back received characters
EVK-MIMX8MQ
Hardware requirements
Micro USB cable
MIMX8MQ6-EVK board
J-Link Debug Probe
12V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 12V power supply and J-Link Debug Probe to the board, switch SW701 to power on the board
Connect a USB cable between the host PC and the J1701 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
Set any baud rate in your terminal, and send character a or A to board, then
When the demo runs successfully, the log would be seen on the debug terminal like:
UART has detect one character A
Baud rate has been set automatic!
Board will send back received characters