powerdown

Overview

This Power demo application allows each of the various low mode modes to be selected, using a simple user interface via the serial port. The example can test below sleep modes (Deep sleep is not implemented with new API): 1 - PM_POWER_DOWN 2 - PM_DEEP_DOWN