MCUXpresso SDK Documentation

lpc_dac_dma

lpc_dac_dma#

Overview#

The dac_dma example shows how to use DAC with dma and produce an arbitrary, user-defined waveform of selectable frequency.The output can be observed with an oscilloscope.

When the DAC’s double-buffer feature is enabled, any write to the CR register will only load the pre-buffer, which shares its register address with the CR register. The CR itself will be loaded from the pre-buffer whenever the counter reaches zero and the DMA request would be raised. At the same time the counter is reloaded with the COUNTVAL register value. user-defined waveform array would be transfered to pre-buffer in order by DMA.

Supported Boards#