enet_txrx_rxpoll#
Overview#
The enet_rxtx_rxinterrupt example shows the simplest way to use ENET functional tx/rx API for simple frame receive and transmit.
This example shows how to initialize the ENET.
How to use ENET to receive frame in polling and to transmit frame.
The example transmits 20 number broadcast frame, print the number and the mac address of the recieved frames.
Supported Boards#
LPCXpresso54628
Hardware requirements
Mini/micro USB cable
LPCXpresso54628 board
Personal Computer
Loopback network cable RJ45 standard
Board settings
For LPCXpresso54628 V2.0:JP11 and JP12 1-2 on.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert loopback network cable to Ethernet RJ45 port.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Make loopback network cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Running the demo
The log below shows example output of the example in the terminal window:
ENET example start.
Transmission start now!
The 1-th frame transmitted success!
The 2-th frame transmitted success!
The 3-th frame transmitted success!
The 4-th frame transmitted success!
The 5-th frame transmitted success!
The 6-th frame transmitted success!
The 7-th frame transmitted success!
The 8-th frame transmitted success!
The 9-th frame transmitted success!
The 10-th frame transmitted success!
The 11-th frame transmitted success!
The 12-th frame transmitted success!
The 13-th frame transmitted success!
The 14-th frame transmitted success!
The 15-th frame transmitted success!
The 16-th frame transmitted success!
The 17-th frame transmitted success!
The 18-th frame transmitted success!
The 19-th frame transmitted success!
The 20-th frame transmitted success!
One frame received. the length 346
Dest Address ff:ff:ff:ff:ff:ff Src Address 00:23:24:9d:33:de
One frame received. the length 64
Dest Address ff:ff:ff:ff:ff:ff Src Address 00:23:24:9d:33:de
One frame received. the length 64
Dest Address ff:ff:ff:ff:ff:ff Src Address 00:23:24:9d:33:de
...
LPCXpresso54S018
Hardware requirements
Mini/micro USB cable
LPCXpresso54S018 board
Personal Computer
Loopback network cable RJ45 standard
Board settings
For LPCXpresso54S018 V2.0:JP11 and JP12 1-2 on.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert loopback network cable to Ethernet RJ45 port.
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Make loopback network cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Running the demo
This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:
Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”
This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):
a. Open SEGGER J-FLASH Lite, select device LPC54S018.
b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)
c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
The log below shows example output of the example in the terminal window:
ENET example start.
Transmission start now!
The 1-th frame transmitted success!
The 2-th frame transmitted success!
The 3-th frame transmitted success!
The 4-th frame transmitted success!
The 5-th frame transmitted success!
The 6-th frame transmitted success!
The 7-th frame transmitted success!
The 8-th frame transmitted success!
The 9-th frame transmitted success!
The 10-th frame transmitted success!
The 11-th frame transmitted success!
The 12-th frame transmitted success!
The 13-th frame transmitted success!
The 14-th frame transmitted success!
The 15-th frame transmitted success!
The 16-th frame transmitted success!
The 17-th frame transmitted success!
The 18-th frame transmitted success!
The 19-th frame transmitted success!
The 20-th frame transmitted success!
One frame received. the length 346
Dest Address ff:ff:ff:ff:ff:ff Src Address 28:f1: e:12:1f:10
One frame received. the length 64
Dest Address ff:ff:ff:ff:ff:ff Src Address 28:f1: e:12:1f:10
One frame received. the length 64
Dest Address ff:ff:ff:ff:ff:ff Src Address 28:f1: e:12:1f:10
...
LPCXpresso54S018M
Hardware requirements
Mini/micro USB cable
LPCXpresso54S018M board
Personal Computer
Loopback network cable RJ45 standard
Board settings
For LPCXpresso54S018M V2.0:JP11, JP12, JP14 and JP15 1-2 on.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert loopback network cable to Ethernet RJ45 port.
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Make loopback network cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Running the demo
This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:
Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”
This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):
a. Open SEGGER J-FLASH Lite, select device LPC54S018M.
b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)
c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
The log below shows example output of the example in the terminal window:
ENET example start.
Transmission start now!
The 1-th frame transmitted success!
The 2-th frame transmitted success!
The 3-th frame transmitted success!
The 4-th frame transmitted success!
The 5-th frame transmitted success!
The 6-th frame transmitted success!
The 7-th frame transmitted success!
The 8-th frame transmitted success!
The 9-th frame transmitted success!
The 10-th frame transmitted success!
The 11-th frame transmitted success!
The 12-th frame transmitted success!
The 13-th frame transmitted success!
The 14-th frame transmitted success!
The 15-th frame transmitted success!
The 16-th frame transmitted success!
The 17-th frame transmitted success!
The 18-th frame transmitted success!
The 19-th frame transmitted success!
The 20-th frame transmitted success!
One frame received. the length 346
Dest Address ff:ff:ff:ff:ff:ff Src Address 28:f1: e:12:1f:10
One frame received. the length 64
Dest Address ff:ff:ff:ff:ff:ff Src Address 28:f1: e:12:1f:10
One frame received. the length 64
Dest Address ff:ff:ff:ff:ff:ff Src Address 28:f1: e:12:1f:10
...