i2c_polling_transfer_slave
Overview
The i2c_polling_transfer_slave example shows how to use i2c driver as slave to do board to board transfer with a polling master:
In this example, one i2c instance as slave and another i2c instance on the other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.