lpi2c_polling_b2b_slave#
Overview#
The lpi2c_polling_b2b_slave example shows how to use lpi2c driver as slave to do board to board transfer with a polling master:
In this example, one lpi2c instance as slave and another lpi2c instance on the other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.
Supported Boards#
EVK9-MIMX8ULP
Hardware requirements
Micro USB cable
two MIMX8ULP-EVK/EVK9 boards
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C0 pins of MASTER_BOARD are connected with LPI2C0 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
I2C0_SCL J20-10 I2C0_SCL J20-10
I2C0_SDA J20-9 I2C0_SDA J20-9
GND GND
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
IMX952LPD5EVK-19
Hardware requirements
Micro USB cable
two IMX952-EVK boards
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connection as below:
MASTER(LPI2C6) connect to SLAVE(LPI2C6)
Pin Name Board Location Pin Name Board Location
SCL J22 pin 3 SCL J22 pin 3
SDA J22 pin 5 SDA J22 pin 5
GND J22 pin 7 GND J22 pin 7
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
EVKB-IMXRT1050
Hardware requirements
Mini/micro USB cable
Two EVKB-IMXRT1050 board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J23-5 LPI2C1_SCL J23-5
LPI2C1_SDA J23-6 LPI2C1_SDA J23-6
GND J24-7 GND J24-7
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MIMXRT1060-EVKB
Hardware requirements
Mini/micro USB cable
Two MIMXRT1060-EVKB board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J33-6 LPI2C1_SCL J33-6
LPI2C1_SDA J33-5 LPI2C1_SDA J33-5
GND J17-7 GND J17-7
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MIMXRT1170-EVKB
Hardware requirements
Mini/micro USB cable
Two MIMXRT1170-EVKB board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J26-12 LPI2C1_SCL J26-12
LPI2C1_SDA J26-10 LPI2C1_SDA J26-10
GND J10-14 GND J10-14
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MIMXRT1060-EVKC
Hardware requirements
Mini/micro USB cable
Two MIMXRT1060-EVKC board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J33-6 LPI2C1_SCL J33-6
LPI2C1_SDA J33-5 LPI2C1_SDA J33-5
GND J17-7 GND J17-7
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-IMXRT1152
Hardware requirements
Type-C USB cable
Two FRDM-IMXRT1152 board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J47-12 LPI2C1_SCL J47-12
LPI2C1_SDA J47-10 LPI2C1_SDA J47-10
GND J47-1 GND J47-1
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
EVK-MCIMX7ULP
Hardware requirements
Micro USB cable
two MCIMX7ULP-EVK boards
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C3 pins of MASTER_BOARD are connected with LPI2C3 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
I2C3_SCL TP24 I2C3_SCL TP24
I2C3_SDA TP26 I2C3_SDA TP26
GND GND
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW1 to power on the board.
Connect a micro USB cable between the host PC and the J6 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
End of LPI2C example .
EVK-MIMX8ULP
Hardware requirements
Micro USB cable
two MIMX8ULP-EVK/EVK9 boards
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C0 pins of MASTER_BOARD are connected with LPI2C0 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
I2C0_SCL J20-10 I2C0_SCL J20-10
I2C0_SDA J20-9 I2C0_SDA J20-9
GND GND
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
EVK-MIMXRT1010
Hardware requirements
Mini/micro USB cable
Two EVK-MIMXRT1010 board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J57-20 LPI2C1_SCL J57-20
LPI2C1_SDA J57-18 LPI2C1_SDA J57-18
GND J57-14 GND J57-14
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
EVK-MIMXRT1015
Hardware requirements
Mini/micro USB cable
Two EVK-MIMXRT1015 board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J18-6 LPI2C1_SCL J18-6
LPI2C1_SDA J18-5 LPI2C1_SDA J18-5
GND J19-7 GND J19-7
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
EVK-MIMXRT1020
Hardware requirements
Mini/micro USB cable
Two EVK-MIMXRT1020 board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J18-6 LPI2C1_SCL J18-6
LPI2C1_SDA J18-5 LPI2C1_SDA J18-5
GND J19-7 GND J19-7
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
MIMXRT1024-EVK
Hardware requirements
Mini/micro USB cable
Two MIMXRT1024-EVK boards
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J18-12 LPI2C1_SCL J18-12
LPI2C1_SDA J18-10 LPI2C1_SDA J18-10
GND J19-14 GND J19-14
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
MIMXRT1040-EVK
Hardware requirements
Mini/micro USB cable
Two MIMXRT1040-EVK board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J17-10 LPI2C1_SCL J17-10
LPI2C1_SDA J17-9 LPI2C1_SDA J17-9
GND J17-7 GND J17-7
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
EVK-MIMXRT1064
Hardware requirements
Mini/micro USB cable
Two EVK-MIMXRT1064 board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J23-6 LPI2C1_SCL J23-6
LPI2C1_SDA J23-5 LPI2C1_SDA J23-5
GND J24-7 GND J24-7
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MIMXRT1160-EVK
Hardware requirements
Mini/micro USB cable
Two MIMXRT1160-EVK board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J26-12 LPI2C1_SCL J26-12
LPI2C1_SDA J26-10 LPI2C1_SDA J26-10
GND J10-14 GND J10-14
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MIMXRT1180-EVK
Hardware requirements
Mini/micro USB cable
Two MIMXRT1180-EVK board
Personal Computer
Board settings
Remove R79, R80 LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C2 pins of MASTER_BOARD are connected with LPI2C2 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C2_SCL J44-20 LPI2C2_SCL J44-20
LPI2C2_SDA J44-18 LPI2C2_SDA J44-18
GND J44-19 GND J44-19
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-K32L2A4S
Hardware requirements
Mini USB cable
Two FRDM-K32L2A4S boards
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J4-12 LPI2C1_SCL J4-12
LPI2C1_SDA J4-10 LPI2C1_SDA J4-10
GND J3-14 GND J3-14
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
End of LPI2C example .
FRDM-K32L3A6
Hardware requirements
Micro USB cable
Two FRDM-K32L3A6 boards
Personal Computer
Board settings
To make lpi2c example work(M4), connections needed to be as follows:
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J1-10(PTB14) LPI2C1_SCL J1-10(PTB14)
LPI2C1_SDA J2-6(PTB6) LPI2C1_SDA J2-6(PTB6)
GND J2-14 GND J2-14
To make lpi2c example work(M0), connections needed to be as follows:
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C3_SCL J3-15(PTB15) LPI2C3_SCL J3-15(PTB15)
LPI2C3_SDA J3-13(PTB16) LPI2C3_SDA J3-13(PTB16)
GND J2-14 GND J2-14
Prepare the Demo
Connect a micro USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for JLink serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following message shows in the terminal if the example runs successfully.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-KE15Z
Hardware requirements
Micro USB cable
Two FRDM-KE15Z boards
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C0 pins of MASTER_BOARD are connected with LPI2C0 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C0_SCL J4-12 LPI2C0_SCL J4-12
LPI2C0_SDA J4-10 LPI2C0_SDA J4-10
GND J3-14 GND J3-14
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
End of LPI2C example .
FRDM-KE16Z
Hardware requirements
Micro USB cable
Two FRDM-KE16Z boards
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C0 pins of MASTER_BOARD are connected with LPI2C0 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C0_SCL J2-20 LPI2C0_SCL J2-20
LPI2C0_SDA J2-18 LPI2C0_SDA J2-18
GND J2-14 GND J2-14
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
End of LPI2C example .
FRDM-KE17Z
Hardware requirements
Micro USB cable
Two FRDM-KE17Z boards
Personal Computer
Board settings
LPI2C two boards:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C0 pins of MASTER_BOARD are connected with LPI2C0 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C0_SCL J2-20 LPI2C0_SCL J2-20
LPI2C0_SDA J2-18 LPI2C0_SDA J2-18
GND J2-14 GND J2-14
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
End of LPI2C example .
FRDM-KE17Z512
Hardware requirements
Micro USB cable
Two FRDM-KE17Z512 boards
Personal Computer
Board settings
LPI2C two boards:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C0 pins of MASTER_BOARD are connected with LPI2C0 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C0_SCL J2-20 LPI2C0_SCL J2-20
LPI2C0_SDA J2-18 LPI2C0_SDA J2-18
GND J2-14 GND J2-14
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board EDMA example -- Master transfer.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Receive sent data from slave :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXA153
Hardware requirements
Type-C USB cable
FRDM-MCXA153 board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
LPI2C:
MASTER(LPI2C0) connect to SLAVE(LPI2C0)
Pin Name Board Location Pin Name Board Location
SDA J5 pin 6 SDA J5 pin 6
SCL J5 pin 5 SCL J5 pin 5
GND J5 pin 8 GND J5 pin 8
Other jumpers keep default configuration.
Prepare the Demo
Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXA156
Hardware requirements
Type-C USB cable
FRDM-MCXA156 board
Personal Computer
Board settings
MASTER(LPI2C0) connect to SLAVE(LPI2C3)
LPI2C0 SCL(P0_17,J2-20) --> LPI2C3 SCL(P3_27,J5_5)
LPI2C0 SDA(P0_16,J2-18) --> LPI2C3 SDA(P3_28,J5_6)
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXA346
Hardware requirements
Type-C USB cable
FRDM-MCXA346 board
Personal Computer
Board settings
MASTER(LPI2C2) connect to SLAVE(LPI2C2)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 20 SCL J2 pin 20
SDA J2 pin 18 SDA J2 pin 18
GND J2 pin 14 GND J2 pin 14
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXE247
Hardware requirements
USB-C cable
Two FRDM-MCXE247 boards
Personal Computer
Board settings
LPI2C two boards:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with LPI2C1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J2-20 LPI2C1_SCL J2-20
LPI2C1_SDA J2-18 LPI2C1_SDA J2-18
GND J2-14 GND J2-14
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board EDMA example -- Master transfer.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Receive sent data from slave :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXN236
Overview
The lpi2c_polling_b2b_slave example shows how to use lpi2c driver as slave to do board to board transfer with a polling master:
In this example, one lpi2c instance as slave and another lpi2c instance on the other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.
Toolchain supported
IAR embedded Workbench 9.30.1
MCUXpresso 11.6.0
Hardware requirements
Type-C USB cable
FRDM-MCXN236 board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C2) connect to SLAVE(LPI2C2)
Pin Name Board Location Pin Name Board Location
SCL J5 pin 5 SCL J5 pin 5
SDA J5 pin 6 SDA J5 pin 6
GND J5 pin 8 GND J5 pin 8
Other jumpers keep default configuration.
Prepare the Demo
Connect the type-c and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXN947
Overview
The lpi2c_polling_b2b_slave example shows how to use lpi2c driver as slave to do board to board transfer with a polling master:
In this example, one lpi2c instance as slave and another lpi2c instance on the other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.
Toolchain supported
IAR embedded Workbench 9.30.1
MCUXpresso 11.6.0
Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C2) connect to SLAVE(LPI2C2)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 20 SCL J2 pin 20
SDA J2 pin 18 SDA J2 pin 18
GND J2 pin 14 GND J2 pin 14
Other jumpers keep default configuration.
Prepare the Demo
Connect the type-c and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXN947T
Overview
The lpi2c_polling_b2b_slave example shows how to use lpi2c driver as slave to do board to board transfer with a polling master:
In this example, one lpi2c instance as slave and another lpi2c instance on the other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.
Toolchain supported
IAR embedded Workbench 9.30.1
MCUXpresso 11.6.0
Hardware requirements
Type-C USB cable
FRDM-MCXN947T board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C2) connect to SLAVE(LPI2C2)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 20 SCL J2 pin 20
SDA J2 pin 18 SDA J2 pin 18
GND J2 pin 14 GND J2 pin 14
Other jumpers keep default configuration.
Prepare the Demo
Connect the type-c and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXW71
Hardware requirements
Type-C USB cable
FRDM-MCXW71 Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SDA J2 pin 2 SDA J2 pin 2
SCL J2 pin 1 SCL J2 pin 1
Other jumpers keep default configuration.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MCX-W71-EVK
Hardware requirements
Type-C USB cable
MCX-W71-EVK Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SDA J2 pin 3 SDA J2 pin 3
SCL J2 pin 1 SCL J2 pin 1
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXW72
Hardware requirements
Type-C USB cable
FRDM-MCXW72 Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SDA J2 pin 2 SDA J2 pin 2
SCL J2 pin 1 SCL J2 pin 1
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
IMX95LPD5EVK-19
Hardware requirements
Micro USB cable
two IMX95LPD5-EVK boards
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connection as below:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SCL J22 pin 3 SCL J22 pin 3
SDA J22 pin 5 SDA J22 pin 5
GND J22 pin 7 GND J22 pin 7
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-IMX95
Hardware requirements
Micro USB cable
two FRDM-IMX95 boards
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connection as below:
MASTER(LPI2C6) connect to SLAVE(LPI2C6)
Pin Name Board Location Pin Name Board Location
SCL J19 pin 3 SCL J19 pin 3
SDA J19 pin 5 SDA J19 pin 5
GND J19 pin 9 GND J19 pin 9
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-IMX952
Hardware requirements
Micro USB cable
two IMX952-EVK boards
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connection as below:
MASTER(LPI2C6) connect to SLAVE(LPI2C6)
Pin Name Board Location Pin Name Board Location
SCL J18 pin 5 SCL J18 pin 5
SDA J18 pin 3 SDA J18 pin 3
GND J18 pin 6 GND J18 pin 6
Note: J18 is the 40-PIN GPIO HDR expansion connector. - J18-Pin5: LPI2C6_SCL (GPIO_IO03) - J18-Pin3: LPI2C6_SDA (GPIO_IO02) - J18-Pin6: Common Ground (any GND pin on J18 can be used) - Pull-up resistors: 2.2kΩ @ 3.3V (built-in, no external pull-ups needed) - Each board must be powered independently - No IO expander configuration required for this example
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-IMX937
Hardware requirements
Micro USB cable
two FRDM-IMX937 boards
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connection as below:
MASTER(LPI2C6) connect to SLAVE(LPI2C6)
Pin Name Board Location Pin Name Board Location
SCL J19 pin 3 SCL J19 pin 3
SDA J19 pin 5 SDA J19 pin 5
GND J19 pin 9 GND J19 pin 9
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
KW45B41Z-EVK
Hardware requirements
Mini/micro USB cable
KW45B41Z-EVK Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SDA J2 pin 9 SDA J2 pin 9
SCL J2 pin 10 SCL J2 pin 10
Other jumpers keep default configuration.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
KW47-EVK
Hardware requirements
Type-C USB cable
KW47-EVK Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SDA J2 pin 3 SDA J2 pin 3
SCL J2 pin 1 SCL J2 pin 1
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MCIMX93AUTO-EVK
Hardware requirements
USB Type-C cable
two MCIMX93AUTO-EVK boards
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connection as below:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SCL J17 pin 16 SCL J17 pin 16
SDA J17 pin 18 SDA J17 pin 18
GND J17 pin 29 GND J17 pin 29
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.
Connect a USB Type-C cable between the host PC and the J26 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MCIMX93-EVK
Hardware requirements
USB Type-C cable
two MCIMX93-EVK boards
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connection as below:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SCL J1005 pin 3 SCL J1005 pin 3
SDA J1005 pin 5 SDA J1005 pin 5
GND J1005 pin 7 GND J1005 pin 7
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MCIMX93W-EVK
Hardware requirements
USB Type-C cable
two MCIMX93W-EVK boards
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connection as below:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SCL J1005 pin 3 SCL J1005 pin 3
SDA J1005 pin 5 SDA J1005 pin 5
GND J1005 pin 7 GND J1005 pin 7
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MCIMX93-QSB
Hardware requirements
USB Type-C cable
two MCIMX93-QSB boards
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connection as below:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SCL J1406 pin 3 SCL J1406 pin 3
SDA J1406 pin 5 SDA J1406 pin 5
GND J1406 pin 7 GND J1406 pin 7
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1708 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MCX-N5XX-EVK
Overview
The lpi2c_polling_b2b_slave example shows how to use lpi2c driver as slave to do board to board transfer with a polling master:
In this example, one lpi2c instance as slave and another lpi2c instance on the other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.
Toolchain supported
IAR embedded Workbench 9.30.1
MCUXpresso 11.6.0
Hardware requirements
Mini/micro USB cable
MCX-N9xx-EVK board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C2) connect to SLAVE(LPI2C2)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 20 SCL J2 pin 20
SDA J2 pin 18 SDA J2 pin 18
GND J2 pin 14 GND J2 pin 14
Other jumpers keep default configuration.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MCX-N9XX-EVK
Overview
The lpi2c_polling_b2b_slave example shows how to use lpi2c driver as slave to do board to board transfer with a polling master:
In this example, one lpi2c instance as slave and another lpi2c instance on the other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.
Toolchain supported
IAR embedded Workbench 9.30.1
MCUXpresso 11.6.0
Hardware requirements
Mini/micro USB cable
MCX-N9xx-EVK board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C2) connect to SLAVE(LPI2C2)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 20 SCL J2 pin 20
SDA J2 pin 18 SDA J2 pin 18
GND J2 pin 14 GND J2 pin 14
Other jumpers keep default configuration.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MCX-W72-EVK
Hardware requirements
Type-C USB cable
MCX-W72-EVK Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SDA J2 pin 3 SDA J2 pin 3
SCL J2 pin 1 SCL J2 pin 1
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MIMXRT700-EVK
Hardware requirements
Micro USB cable
Target microcontroller board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C8) connect to SLAVE(LPI2C8)
Pin Name Board Location Pin Name Board Location
SCL J11 pin 5 SCL J11 pin 5
SDA J11 pin 6 SDA J11 pin 6
GND J11 pin 8 GND J11 pin 8
Other jumpers keep default configuration.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXE31B
Hardware requirements
Type-C USB cable
FRDM-MCXE31B board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C_1 pins of MASTER_BOARD are connected with LPI2C_1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C_1_SCL J2-20 LPI2C_1_SCL J2-20
LPI2C_1_SDA J2-18 LPI2C_1_SDA J2-18
GND J2-14 GND J2-14
Prepare the Demo
Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXE32B
Hardware requirements
Type-C USB cable
FRDM-MCXE32B board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C_1 pins of MASTER_BOARD are connected with LPI2C_1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C_1_SCL J2-20 LPI2C_1_SCL J2-20
LPI2C_1_SDA J2-18 LPI2C_1_SDA J2-18
GND J2-14 GND J2-14
Prepare the Demo
Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXL255
Hardware requirements
Type-C USB cable
FRDM-MCXL255 board
Personal Computer
Board settings
LPI2C:
CM33
MASTEE(I2C0) connect to SLAVE(I2C0)
Pin Name Board Location Pin Name Board Location
LPI2C0_SCL J5-5 LPI2C0_SCL J5-5
LPI2C0_SDA J5-6 LPI2C0_SDA J5-6
GND J5-8 GND J5-8
CM0PLUS:
MASTER(AON__I2C0) connect to SLAVE(AON__I2C0)
Pin Name Board Location Pin Name Board Location
AON__I2C0_SCL J2-9 AON__I2C0_SCL J2-9
AON__I2C0_SDA J2-7 AON__I2C0_SDA J2-7
GND J2-14 GND J2-14
Make sure you have solder bridges SJ1 and SJ2 set to
2-1 for the main core (cm33)
2-3 for AON core (cm0+)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port (J16) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXA174
Hardware requirements
Type-C USB cable
FRDM-MCXA174 board
Personal Computer
Board settings
MASTER(LPI2C0) connect to SLAVE(LPI2C0)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 20 SCL J2 pin 20
SDA J2 pin 18 SDA J2 pin 18
GND J2 pin 14 GND J2 pin 14
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXA344
Hardware requirements
Type-C USB cable
FRDM-MCXA344 board
Personal Computer
Board settings
MASTER(LPI2C0) connect to SLAVE(LPI2C0)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 20 SCL J2 pin 20
SDA J2 pin 18 SDA J2 pin 18
GND J2 pin 14 GND J2 pin 14
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
KW47-LOC
Hardware requirements
Type-C USB cable
KW47-LOC Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 5 SCL J2 pin 5
SDA J2 pin 6 SDA J2 pin 6
Short the JP24-2 and JP24-3 with the jumper, other jumpers keep default configuration.
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
MCXW72-LOC
Hardware requirements
Type-C USB cable
MCXW72-LOC Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 5 SCL J2 pin 5
SDA J2 pin 6 SDA J2 pin 6
Short the JP24-2 and JP24-3 with the jumper, other jumpers keep default configuration.
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-IMXRT1186
Hardware requirements
Type-C USB cable
Two FRDM-IMXRT1186 boards
Personal Computer
Board settings
Change Jumper J31 from 1-2 to 2-3, Jumper J35 from 1-2 to 2-3. LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C3 pins of MASTER_BOARD are connected with LPI2C3 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C3_SCL J51-12 LPI2C3_SCL J51-12
LPI2C3_SDA J51-10 LPI2C3_SDA J51-10
GND J51-1 GND J51-1
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXA266
Hardware requirements
Type-C USB cable
FRDM-MCXA266 board
Personal Computer
Board settings
MASTER(LPI2C2) connect to SLAVE(LPI2C2)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 20 SCL J2 pin 20
SDA J2 pin 18 SDA J2 pin 18
GND J2 pin 14 GND J2 pin 14
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXA366
Hardware requirements
Type-C USB cable
FRDM-MCXA366 board
Personal Computer
Board settings
MASTER(LPI2C2) connect to SLAVE(LPI2C2)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 20 SCL J2 pin 20
SDA J2 pin 18 SDA J2 pin 18
GND J2 pin 14 GND J2 pin 14
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXA577
Hardware requirements
Type-C USB cable
FRDM-MCXA577 board
Personal Computer
Board settings
MASTER(LPI2C0) connect to SLAVE(LPI2C0)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 20 SCL J2 pin 20
SDA J2 pin 18 SDA J2 pin 18
GND J2 pin 14 GND J2 pin 14
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXC162
Hardware requirements
Type-C USB cable
FRDM-MCXC162 board
Personal Computer
Board settings
MASTER(LPI2C0) connect to SLAVE(LPI2C0)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 20 SCL J2 pin 20
SDA J2 pin 18 SDA J2 pin 18
GND J2 pin 14 GND J2 pin 14
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-KW43
Hardware requirements
Type-C USB cable
FRDM-KW43 Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SDA J24 pin 5 SDA J24 pin 5
SCL J24 pin 6 SCL J24 pin 6
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J28.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXW70
Hardware requirements
Type-C USB cable
FRDM-MCXW70 Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
MASTER(LPI2C1) connect to SLAVE(LPI2C1)
Pin Name Board Location Pin Name Board Location
SDA J24 pin 5 SDA J24 pin 5
SCL J24 pin 6 SCL J24 pin 6
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J28.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .
FRDM-MCXA287
Hardware requirements
Type-C USB cable
FRDM-MCXA287 board
Personal Computer
Board settings
MASTER(LPI2C0) connect to SLAVE(LPI2C0)
Pin Name Board Location Pin Name Board Location
SCL J2 pin 20 SCL J2 pin 20
SDA J2 pin 18 SDA J2 pin 18
GND J2 pin 14 GND J2 pin 14
Other jumpers keep default configuration.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .