lpspi_edma_transfer#
Overview#
The lpspi_edma example shows how to use LPSPI driver in edma way:
In this example , one lpspi instance used as LPSPI master and another lpspi instance used as LPSPI slave .
LPSPI master send/received data to/from LPSPI slave in edma . (LPSPI Slave using edma to receive/send the data)
Running the demo#
When the example runs successfully, you can see the similar information from the terminal as below.
LPSPI edma example start. This example use one lpspi instance as master and another as slave on one board. Both master and slave use edma way. Please make sure you make the correct line connection. Basically, the connection is: LPSPI_master – LPSPI_slave CLK – CLK PCS – PCS SOUT – SIN SIN – SOUT
This is LPSPI slave edma transfer completed callback. It’s a successful transfer.
LPSPI transfer all data matched!
End of example.
Supported Boards#
IMX943-EVK
Hardware requirements
Mini/micro USB cable
IMX943-EVK board
Personal Computer
Board settings
LPSPI:
MASTER(LPSPI3) connect to SLAVE(LPSPI8)
Pin Name Board Location Pin Name Board Location
SOUT J47-8 SIN J43-10
SIN J47-10 SOUT J43-8
SCK J47-12 SCK J43-12
PCS0 J47-6 PCS0 J43-6
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
LPSPI edma example start.
This example use one lpspi instance as master and another as slave on one board.
Both master and slave use edma way.
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- LPSPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
This is LPSPI slave edma transfer completed callback.
It's a successful transfer.
LPSPI transfer all data matched!
End of example.