MCUXpresso SDK Documentation

mcxw23_romapi_flash

mcxw23_romapi_flash#

Overview#

The IAP Flash project is a simple demonstration program of the SDK IAP Flash driver. A message is printed on the UART terminal when various operations are performed on Flash memory.

Running the demo#

The log below shows example output of the IAP Flash demo in the terminal window:

        ----- Flash driver IAP Demo Application -----
Initializing Flash driver...
Flash Init done with success !
        PflashTotalSize = 1040384
        PflashSectorSize = 8192
        PflashPageSize = 128
        PflashBlockSize = 1040384
        PflashBlockCount = 1
        PflashBlockBaseAddr = 0
        PflashSystemFreqMHz = 32
Flash Properties printed with success !
Working on Flash Address : 0xFC000
Finished 'Erase/Write' Scenario with success !
Finished 'Read/Modify/Write' Scenario with success !
Executing interrupts from RAM during flash operations: USER LED should start blinking ..
Finished FlashEraseProgramDuringRAMInterrupt with success !
1.Going from 32MHz (high freq) to 12MHz (low freq)
2.Going from 12MHz (low freq)  to 32MHz (high freq)
3.Going from 32MHz (high freq) to 12MHz (low freq)
Finished FlashUpdateWaitStatesAccordingToMainClk with success !

## Supported Boards

````{container} board-selector

```{container} board-setup
:name: board-frdmmcxw23

##### FRDM-MCXW23

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXW23 Board
- Personal Computer

##### Board settings
Use the default jumper settings.

##### Prepare the Demo
1.  Connect a USB cable between the host PC and the FRDM board J10.
2.  Open a serial terminal with the following settings
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Build and download the application
4.  Start a debug session or press the reset button

##### Running the demo
The log below shows example output of the IAP Flash demo in the terminal window:
----- Flash driver IAP Demo Application -----

Initializing Flash driver… Flash Init done with success ! PflashTotalSize = 1040384 PflashSectorSize = 8192 PflashPageSize = 128 PflashBlockSize = 1040384 PflashBlockCount = 1 PflashBlockBaseAddr = 0 PflashSystemFreqMHz = 32 Flash Properties printed with success ! Working on Flash Address : 0xFC000 Finished ‘Erase/Write’ Scenario with success ! Finished ‘Read/Modify/Write’ Scenario with success ! Executing interrupts from RAM during flash operations: USER LED should start blinking .. Finished FlashEraseProgramDuringRAMInterrupt with success ! 1.Going from 32MHz (high freq) to 12MHz (low freq) 2.Going from 12MHz (low freq) to 32MHz (high freq) 3.Going from 32MHz (high freq) to 12MHz (low freq) Finished FlashUpdateWaitStatesAccordingToMainClk with success ! FLASH_CheckECC found no ECC errors !


```{container} board-setup
:name: board-mcxw23evk

##### MCXW23-EVK

##### Hardware requirements
- Mini/micro USB cable
- MCXW23-EVK Board
- Personal Computer

##### Board settings
No special settings are required.

##### Prepare the Demo
1.  Connect a USB cable between the host PC and the EVK board J33.
2.  Open a serial terminal with the following settings
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Build and download the application
4.  Start a debug session or press the reset button

##### Running the demo
The log below shows example output of the IAP Flash demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
 	----- Flash driver IAP Demo Application -----
Initializing Flash driver...
Flash Init done with success !
	PflashTotalSize = 1040384
	PflashSectorSize = 8192
	PflashPageSize = 128
	PflashBlockSize = 1040384
	PflashBlockCount = 1
	PflashBlockBaseAddr = 0
	PflashSystemFreqMHz = 32
Flash Properties printed with success !
Working on Flash Address : 0xFC000 
Finished 'Erase/Write' Scenario with success !
Finished 'Read/Modify/Write' Scenario with success !
Executing interrupts from RAM during flash operations: USER LED should start blinking ..
Finished FlashEraseProgramDuringRAMInterrupt with success !
1.Going from 32MHz (high freq) to 12MHz (low freq)
2.Going from 12MHz (low freq) to 32MHz (high freq)
3.Going from 32MHz (high freq) to 12MHz (low freq)
Finished FlashUpdateWaitStatesAccordingToMainClk with success !
FLASH_CheckECC found no ECC errors !