pxp_lcdif_handshake

Overview

The PXP LCDIF hand shake project shows how to enable the hand shake between PXP and LCDIF. If this example runs correctly, you will see two rectangles moving in the screen. One rectangle is process surface output, and the other is alpha surface output, the overlay region color is OR’ed value of process surface and alpha surface.

NOTE: This example must run continously to get the right result, breaking during debug will results to handshake fail. Because the PXP must be started before every LCD frame, if system is halt, the PXP does not start correctly.

Supported Boards